Error when using S32K14 AutoSAR OS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error when using S32K14 AutoSAR OS

10,599 Views
geweilin
Contributor II

I installed tresos Studio 23.0 , Autosar OS(SW32K14-OS401-RTM-1.0.0 b4.0.98)  and Autosar MCAL(SW32K14-MCAL401-RTMC-1.0.4).

The result is that MCAL is used and tested good.

But when I try to generate OS configuration file(.c,.h), it gives the following 3 error:

1. Failed to run generator "Os_TS_T40D2M4I0R98GeneratorId" (mode: "generate") for module "Os_TS_T40D2M4I0R98"

2. Error in external generator: fatal 0201: 'S32K' target is not supported by your license!
Used generator commandline: C:\EB\tresos23\..\..\NXP\AUTOSAR\S32K_AUTOSAR_OS_4_0_98_RTM_1_0_0\os_ts\eclipse\plugins\Os_TS_T40D2M4I0R98\..\..\..\..\ssc\bin\generator\sg.exe C:\Users\weilin.ge\Desktop\os_sample_sc1\output\generated\epc\project.epc

3. The external generator for module Os_TS_T40D2M4I0R98 terminated with exit code 9
Used generator commandline: C:\EB\tresos23\..\..\NXP\AUTOSAR\S32K_AUTOSAR_OS_4_0_98_RTM_1_0_0\os_ts\eclipse\plugins\Os_TS_T40D2M4I0R98\..\..\..\..\ssc\bin\generator\sg.exe C:\Users\weilin.ge\Desktop\os_sample_sc1\output\generated\epc\project.epc

I want to what's the problem reason? and how to resolve it? 

Thanks.

Tags (3)
12 Replies

10,175 Views
allenlw
Contributor III

the OS generator need a java run enrivonment, so you need to download a JRE from the official site and install it . I think it wil solve your problem.

10,175 Views
qianyanhua
Contributor I

When I use the sample,it's OK;but when I create my project,or change the sample,it's the same error "The external generator for module Os_T40D2M4I0R98 terminated with exit code 7".

0 Kudos
Reply

10,175 Views
allenlw
Contributor III

do you install the JRE like I said before?

0 Kudos
Reply

10,175 Views
qianyanhua
Contributor I

Yes,I did it,but when I create a new project ,the error reappears.

0 Kudos
Reply

10,176 Views
allenlw
Contributor III

I don't know what exactly the problem you meet, but you can find a decimal number at the front end of the error message, then look it up at the 21.4 list of messages in the AUTOSAR_OSS32K_TR, it's a document in the OS installation folder, hope this will help you.

0 Kudos
Reply

10,175 Views
qianyanhua
Contributor I

Yes,before I install JRE, the sample generate is not OK,but after that,it's OK.Error reappears when I use a new project,or change the samle.

[email protected]

0 Kudos
Reply

10,175 Views
xinxin_you
Contributor II

I meet this problem.How to slove it?

0 Kudos
Reply

10,175 Views
江洪秦
Contributor I

I  have the same problem. Do you know how to solve it ?

0 Kudos
Reply

10,173 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

I created ticket with your question for Automotive Software team. The will contact you back directly via email. Please let me know here, if you do not receive reply until end of this week.

Regards,

Martin

0 Kudos
Reply

9,515 Views
Simin
Contributor II

Hi,

        I also have this problem too,and don't know how to solve it,pls support me,thank you very much

Best regards,

simin

0 Kudos
Reply

9,889 Views
lubo_NEW
Contributor III

I meet this problem.How to slove it?

0 Kudos
Reply

10,173 Views
江洪秦
Contributor I

Hi, Martin,

 Could you share the solved method?

0 Kudos
Reply