Error when using S32K14 AutoSAR OS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error when using S32K14 AutoSAR OS

10,903件の閲覧回数
geweilin
Contributor II

I installed tresos Studio 23.0 , Autosar OS(SW32K14-OS401-RTM-1.0.0 b4.0.98)  and Autosar MCAL(SW32K14-MCAL401-RTMC-1.0.4).

The result is that MCAL is used and tested good.

But when I try to generate OS configuration file(.c,.h), it gives the following 3 error:

1. Failed to run generator "Os_TS_T40D2M4I0R98GeneratorId" (mode: "generate") for module "Os_TS_T40D2M4I0R98"

2. Error in external generator: fatal 0201: 'S32K' target is not supported by your license!
Used generator commandline: C:\EB\tresos23\..\..\NXP\AUTOSAR\S32K_AUTOSAR_OS_4_0_98_RTM_1_0_0\os_ts\eclipse\plugins\Os_TS_T40D2M4I0R98\..\..\..\..\ssc\bin\generator\sg.exe C:\Users\weilin.ge\Desktop\os_sample_sc1\output\generated\epc\project.epc

3. The external generator for module Os_TS_T40D2M4I0R98 terminated with exit code 9
Used generator commandline: C:\EB\tresos23\..\..\NXP\AUTOSAR\S32K_AUTOSAR_OS_4_0_98_RTM_1_0_0\os_ts\eclipse\plugins\Os_TS_T40D2M4I0R98\..\..\..\..\ssc\bin\generator\sg.exe C:\Users\weilin.ge\Desktop\os_sample_sc1\output\generated\epc\project.epc

I want to what's the problem reason? and how to resolve it? 

Thanks.

タグ(3)
12 返答(返信)

10,479件の閲覧回数
allenlw
Contributor III

the OS generator need a java run enrivonment, so you need to download a JRE from the official site and install it . I think it wil solve your problem.

10,479件の閲覧回数
qianyanhua
Contributor I

When I use the sample,it's OK;but when I create my project,or change the sample,it's the same error "The external generator for module Os_T40D2M4I0R98 terminated with exit code 7".

0 件の賞賛
返信

10,479件の閲覧回数
allenlw
Contributor III

do you install the JRE like I said before?

0 件の賞賛
返信

10,479件の閲覧回数
qianyanhua
Contributor I

Yes,I did it,but when I create a new project ,the error reappears.

0 件の賞賛
返信

10,480件の閲覧回数
allenlw
Contributor III

I don't know what exactly the problem you meet, but you can find a decimal number at the front end of the error message, then look it up at the 21.4 list of messages in the AUTOSAR_OSS32K_TR, it's a document in the OS installation folder, hope this will help you.

0 件の賞賛
返信

10,479件の閲覧回数
qianyanhua
Contributor I

Yes,before I install JRE, the sample generate is not OK,but after that,it's OK.Error reappears when I use a new project,or change the samle.

[email protected]

0 件の賞賛
返信

10,479件の閲覧回数
xinxin_you
Contributor I

I meet this problem.How to slove it?

0 件の賞賛
返信

10,479件の閲覧回数
江洪秦
Contributor I

I  have the same problem. Do you know how to solve it ?

0 件の賞賛
返信

10,477件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

I created ticket with your question for Automotive Software team. The will contact you back directly via email. Please let me know here, if you do not receive reply until end of this week.

Regards,

Martin

0 件の賞賛
返信

9,819件の閲覧回数
Simin
Contributor II

Hi,

        I also have this problem too,and don't know how to solve it,pls support me,thank you very much

Best regards,

simin

0 件の賞賛
返信

10,193件の閲覧回数
lubo_NEW
Contributor III

I meet this problem.How to slove it?

0 件の賞賛
返信

10,477件の閲覧回数
江洪秦
Contributor I

Hi, Martin,

 Could you share the solved method?

0 件の賞賛
返信