Error in C40_IP Peripherals Drivers in s32 Design Studio

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Error in C40_IP Peripherals Drivers in s32 Design Studio

跳至解决方案
757 次查看
Ajay_R1
Contributor I

I am using S32 Design Studio Platform IDE 3.5 for NXP S32K324 target board. 

I have created a new project with C40_IP Driver from my laptop and I am able to build successfully on my Target Board.

Same project, I shared it to one of my colleague,  it is not working for him and it was throughing error. Finally we cross verified all the software installed(like RTD, Development  package and S32 platform package)on our laptop.

For both of them it was same. But there is a difference in C40_IP driver where I have C40_IP Configuration while my colleague has C40_IP Driver. Please find the attachment, for your reference.

The below screenshot has taken from my Laptop.

Ajay_R1_3-1715765065719.png

 

Below Screenshot has taken from my colleague Laptop.

Ajay_R1_4-1715768993597.png

 

 

 

 

Regards,

Ajay. R

 

 

 

 

0 项奖励
回复
1 解答
711 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Ajay_R1,

You can update your RTD versions to the latest release for RTD 3.0.0 (P10) which include the Mem drivers, or downgrade to RTD 3.0.0 (without patch) for compatibility with the working project. You can look into the release notes for each version to see if these drivers are supported:

Julin_AragnM_0-1715895951311.png

Best regards,
Julián

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
733 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Ajay_R1,

The Fls Driver has been replaced by Mem_InFls/Mem_ExFls to comply with AUTOSAR R21-11. Since NXP still provides the old Fls, Eep and Fee Drivers in parallel, some RTD versions still have these drivers.

Could you share which RTD versions you and your colleague are using?

Best regards,
Julián

0 项奖励
回复
716 次查看
Ajay_R1
Contributor I

Hi @Julián_AragónM ,

I have mentioned the versions in below which we are using.  

S32 Design Studio Platform Package Version 3.5.11

S32K3XX development Package, Version 3.5.8

S32K3XX.P01 RTD AUTOSAR R21-11 VEERSION 3.0.0

S32K3XX RTD AUTOSAR R21-11 VEERSION 3.0.0

The below screenshot has taken from my laptop

Ajay_R1_0-1715868391839.png

The below screenshot has taken from My colleague laptop

Ajay_R1_2-1715868569770.png

If you are required more details please let me know.

 

Regards,

Ajay. R

0 项奖励
回复
712 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Ajay_R1,

You can update your RTD versions to the latest release for RTD 3.0.0 (P10) which include the Mem drivers, or downgrade to RTD 3.0.0 (without patch) for compatibility with the working project. You can look into the release notes for each version to see if these drivers are supported:

Julin_AragnM_0-1715895951311.png

Best regards,
Julián

 

0 项奖励
回复