I am using S32 Design Studio Platform IDE 3.5 for NXP S32K324 target board.
I have created a new project with C40_IP Driver from my laptop and I am able to build successfully on my Target Board.
Same project, I shared it to one of my colleague, it is not working for him and it was throughing error. Finally we cross verified all the software installed(like RTD, Development package and S32 platform package)on our laptop.
For both of them it was same. But there is a difference in C40_IP driver where I have C40_IP Configuration while my colleague has C40_IP Driver. Please find the attachment, for your reference.
The below screenshot has taken from my Laptop.
Below Screenshot has taken from my colleague Laptop.
Regards,
Ajay. R
Solved! Go to Solution.
Hi @Ajay_R1,
You can update your RTD versions to the latest release for RTD 3.0.0 (P10) which include the Mem drivers, or downgrade to RTD 3.0.0 (without patch) for compatibility with the working project. You can look into the release notes for each version to see if these drivers are supported:
Best regards,
Julián
Hi @Ajay_R1,
The Fls Driver has been replaced by Mem_InFls/Mem_ExFls to comply with AUTOSAR R21-11. Since NXP still provides the old Fls, Eep and Fee Drivers in parallel, some RTD versions still have these drivers.
Could you share which RTD versions you and your colleague are using?
Best regards,
Julián
Hi @Julián_AragónM ,
I have mentioned the versions in below which we are using.
S32 Design Studio Platform Package Version 3.5.11
S32K3XX development Package, Version 3.5.8
S32K3XX.P01 RTD AUTOSAR R21-11 VEERSION 3.0.0
S32K3XX RTD AUTOSAR R21-11 VEERSION 3.0.0
The below screenshot has taken from my laptop
The below screenshot has taken from My colleague laptop
If you are required more details please let me know.
Regards,
Ajay. R
Hi @Ajay_R1,
You can update your RTD versions to the latest release for RTD 3.0.0 (P10) which include the Mem drivers, or downgrade to RTD 3.0.0 (without patch) for compatibility with the working project. You can look into the release notes for each version to see if these drivers are supported:
Best regards,
Julián