Error Correcting Code (ECC)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Error Correcting Code (ECC)

跳至解决方案
4,868 次查看
MohamedSalah
Contributor II

Hello All.

I am Working On Some Project on [ S32k312 MCU] Using:
Compiler ==> GHS MultiTool 
Debugger ==> Lauterbach Trace 32 

MCAL Integrator Tool ==> EB Tressos Studio 

The problem is when I Inject Multi Bit Errors using EIM Module to the SRAM0 
The MCU Raises A bus Fault Exception 
While I Followed The Steps in Reference Manual.

I was Waiting to see the ERM Multibit Error ISR To be called but this is not the Case.

I Searched About the problem and Found That XRDC May be restricting access to this RAM Location and may be the reason this fault happens 

but later I found that the XRDC is not Configured From Tressos Studio. 

So Two Questions are there ? 
1) What could be the Reasons to this bus Fault ?
2)How To know Configure XRDC Module in Tressos Studio ? 

Thanks A lot 

0 项奖励
回复
1 解答
4,832 次查看
DanNguyenDuy
NXP Employee
NXP Employee

Hi MohamedSalah,

1. The Bus fault occurred because had a write command to the memory area where EIM was injected error complete.

In some situations, the debugger can cause the bus fault error. So, you can test with turn off the debugger and using blink-led statements to inform the test is successful.

2. To configure XRDC, you can refer to the RTD_RM_UM.pdf file in the RM module in the package.

Best regards,

Dan

在原帖中查看解决方案

2 回复数
4,819 次查看
MohamedSalah
Contributor II

Thanks Dan for your reply 

0 项奖励
回复
4,833 次查看
DanNguyenDuy
NXP Employee
NXP Employee

Hi MohamedSalah,

1. The Bus fault occurred because had a write command to the memory area where EIM was injected error complete.

In some situations, the debugger can cause the bus fault error. So, you can test with turn off the debugger and using blink-led statements to inform the test is successful.

2. To configure XRDC, you can refer to the RTD_RM_UM.pdf file in the RM module in the package.

Best regards,

Dan