Embedded Code Protection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Embedded Code Protection

1,935件の閲覧回数
D_D97
Contributor II

Hello world, 

I am using Design Studio to develop a project on S32k144 microcontroller.

I upload the c code written in the IDE to the microcontroller using the Debug option "project_name_debug_flash_pemicro".
After disconnecting the programmer, resetting the board (or microcontroller) the code starts running.
My question is, is there any chance that anyone who have the microcontroller could extract the c code I uploaded ? or anything related to the code i have uploaded or it is encrypted ? thank you a lot,

Dema

 

#s32k144 #security 

0 件の賞賛
返信
3 返答(返信)

1,911件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @D_D97,

If JTAG/SWD interface is not protected, any user may be able to read out the memory, such as connecting to the MCU or reading the binary, but most likely not the source code, please refer to the following community posts: 
 
The JTAG/SWD interface can be password protected, please refer to this document: [S32K3] Restrict the debug access with a password when HSE is not used.
 
Best regards,
Julián
0 件の賞賛
返信

1,894件の閲覧回数
D_D97
Contributor II
I'm using OpenSDA interface, is it secure ? 
0 件の賞賛
返信

1,877件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @D_D97,

If not enabled, the OpenSDA interface is not secured. Again, you can secure the debug port with password by following the instructions in this community post: [S32K3] Restrict the debug access with a password when HSE is not used.

Best regards,
Julián

0 件の賞賛
返信