ECC RAM initialization and S32DS startup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ECC RAM initialization and S32DS startup

跳至解决方案
6,059 次查看
kef2
Senior Contributor V

Hi

AN12522 states about ECC RAM:

  • 2.2 Used ECC algorithm
    The ECC implementation for the SRAM uses a Modified Hamming Code scheme with 40-bit check base that consists of 32-bits of data plus 8-parity bits.

Clearly RAM initialization should be done in 32-bits aligned word writes. I thought that initializing RAM writing byte by byte could easily trigger ECC error flags set in ERM (I'm using S32K144 and S32K148). But S32DS startup code indeed seems initializing RAM byte by byte:

uint8_t * data_ram;

uint8_t * code_ram;

uint8_t * bss_start;

...

/* Copy initialized data from ROM to RAM */

while (data_rom_end != data_rom)

{

*data_ram = *data_rom;

data_ram++;

data_rom++;

}

/* Copy functions from ROM to RAM */

while (code_rom_end != code_rom)

{

*code_ram = *code_rom;

code_ram++;

code_rom++;

}

/* Clear the zero-initialized data section */

while(bss_end != bss_start)

{

*bss_start = 0;

bss_start++;

}

Since it is told that out of power on SRAM isn't initialized and ECC bits are most likely not OK, I decided to check it. Cloning flash Debug configuration and making debugger not reload flash but connect without reset to running MCU, powering MCU down for a while, then powering on, connecting debugger and inspecting ERM status registers I found that indeed status bits do report ECC problems. Then I added loop code into startup_S32K144.S to step through the rest of startup and figuring out what actually triggers ECC flags. ECC errors start flipping from the first byte by byte initialization loop.

My question are here. "Modified Hamming Code scheme with 40-bit check base that consists of 32-bits of data plus 8-parity bits.". Does it mean that 1) every RAM byte has dedicated 8/4=2 ECC bits? 2) Is it safe to write just single byte to uninitialized RAM DWORD and expect to read the same byte value after writing remaining 3 bytes of the same RAM DWORD?

Thanks

Edward

0 项奖励
回复
1 解答
5,995 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Edward,

The SRAM ECC is initialized in the startup_S32K144.S file and this is done by 32b writes.

I was able to reproduce your test results only when I removed the ECC initialization.

pastedImage_1.png

I don't know which version of S32DS you are using.

As far as I know, the first version of the startup code didn't include the ECC initialization, it was added later.

Regards,

Daniel

在原帖中查看解决方案

3 回复数
5,996 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Edward,

The SRAM ECC is initialized in the startup_S32K144.S file and this is done by 32b writes.

I was able to reproduce your test results only when I removed the ECC initialization.

pastedImage_1.png

I don't know which version of S32DS you are using.

As far as I know, the first version of the startup code didn't include the ECC initialization, it was added later.

Regards,

Daniel

5,995 次查看
kef2
Senior Contributor V

Hi Daniel,

thank You! I started from creating new "S32DS Project from Example". Example projects seem being not updated and  use old startup files. Creating new "S32DS Application Project" I see what you provided in startup*.S file. 

 

Initializing only used locations could make startup bit faster. As well ECC handler could be used to detect unexpected accesses to locations which shouldn't be used (not initialized locations)... But initializing all available RAM is quite good as well.

Regards,

Edward

0 项奖励
回复
5,995 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Edward,

I see, the non-SDK examples haven't been updated.

Let me report that.

Thank you,

BR, Daniel

0 项奖励
回复