When I enable Isr in platform module, then I found the maximum priority only up to 15, if the priority is set to greater than 15, then EB will report a error that the priority out of range. how can I set the priority greater than 15? And I want to know whether I can set the priority group in EB.
Here I use s32k344 and RTD 4.0.0.0
解決済! 解決策の投稿を見る。
 VaneB
		
			VaneB
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi @vivid_
In the S32K3xx Reference Manual, it is stated that there are 16 priority levels configurable in 4 bits in IRQn fields in NVIC IPRn registers.
According to NVIC_SetPriority(), the 4 less significant bits in IRQn fields in NVIC IPRn registers are not implemented.
Whith the above information, the Table 4-18 (Priority grouping) of the ARM Cortex-M7 Devices Generic User Guide, can be understood in this way:
In addition, about priority grouping, a function is also provided, see the following image.
BR, VaneB
 VaneB
		
			VaneB
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi @vivid_
In the S32K3xx Reference Manual, it is stated that there are 16 priority levels configurable in 4 bits in IRQn fields in NVIC IPRn registers.
According to NVIC_SetPriority(), the 4 less significant bits in IRQn fields in NVIC IPRn registers are not implemented.
Whith the above information, the Table 4-18 (Priority grouping) of the ARM Cortex-M7 Devices Generic User Guide, can be understood in this way:
In addition, about priority grouping, a function is also provided, see the following image.
BR, VaneB