Device Name Segger J-Link Debugging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Device Name Segger J-Link Debugging

Jump to solution
7,508 Views
ShinyGreenRobot
Contributor I

Hi

We are attempting to debug a custom hardware based on a S32K142 (FS32K142HAT0MLHT).

Would like to do the debugging with a J-Link Base from Segger in combination with S32 Design Studio for ARM.

When attempting to setup the debug configuration in S32 Design Studio, in the interface that is depicted below, so is there a field called Device name that needs to filled in. What would be suitable to enter in this field when having a S32K142 MCU?

image823.pngimage823.png

Regards SGR

0 Kudos
Reply
1 Solution
7,500 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @ShinyGreenRobot,

In the following link, you can find the list of devices supported by the J-Link debuggers, the name is the one that you need to use in the Device Name box.

Best Regards,

Alexis Andalon

View solution in original post

0 Kudos
Reply
2 Replies
7,501 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @ShinyGreenRobot,

In the following link, you can find the list of devices supported by the J-Link debuggers, the name is the one that you need to use in the Device Name box.

Best Regards,

Alexis Andalon

0 Kudos
Reply
7,496 Views
ShinyGreenRobot
Contributor I

OK thanks found the name S32K142 in the list of devices so will use that device name in the debug configuration.

0 Kudos
Reply