Device Name Segger J-Link Debugging

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Device Name Segger J-Link Debugging

ソリューションへジャンプ
7,697件の閲覧回数
ShinyGreenRobot
Contributor I

Hi

We are attempting to debug a custom hardware based on a S32K142 (FS32K142HAT0MLHT).

Would like to do the debugging with a J-Link Base from Segger in combination with S32 Design Studio for ARM.

When attempting to setup the debug configuration in S32 Design Studio, in the interface that is depicted below, so is there a field called Device name that needs to filled in. What would be suitable to enter in this field when having a S32K142 MCU?

image823.png

Regards SGR

0 件の賞賛
返信
1 解決策
7,689件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @ShinyGreenRobot,

In the following link, you can find the list of devices supported by the J-Link debuggers, the name is the one that you need to use in the Device Name box.

Best Regards,

Alexis Andalon

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
7,690件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @ShinyGreenRobot,

In the following link, you can find the list of devices supported by the J-Link debuggers, the name is the one that you need to use in the Device Name box.

Best Regards,

Alexis Andalon

0 件の賞賛
返信
7,685件の閲覧回数
ShinyGreenRobot
Contributor I

OK thanks found the name S32K142 in the list of devices so will use that device name in the debug configuration.

0 件の賞賛
返信