Default boot mode and Boot pins in S32k142

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Default boot mode and Boot pins in S32k142

跳至解决方案
663 次查看
Jeevansagar
Contributor III

I am working on S32k142 MCU. I want the boot mode to be from Flash.

What is the default Boot Mode in S32k14x MCUs and also i did not found any Boot pins in the Pinout, How is the Boot mode configuration done?

thanks,

jeevan

标记 (1)
0 项奖励
回复
1 解答
649 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Jeevansagar 

S32K1xx devices have only one boot mode - from internal flash from address 0 (0x0 initial SP_main and 0x4 initial PC). There are no other options, so there are no boot pins.

Regards,

Lukas

 

 

 

 

 

 

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
650 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Jeevansagar 

S32K1xx devices have only one boot mode - from internal flash from address 0 (0x0 initial SP_main and 0x4 initial PC). There are no other options, so there are no boot pins.

Regards,

Lukas

 

 

 

 

 

 

 

0 项奖励
回复