Default boot mode and Boot pins in S32k142

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Default boot mode and Boot pins in S32k142

ソリューションへジャンプ
754件の閲覧回数
Jeevansagar
Contributor III

I am working on S32k142 MCU. I want the boot mode to be from Flash.

What is the default Boot Mode in S32k14x MCUs and also i did not found any Boot pins in the Pinout, How is the Boot mode configuration done?

thanks,

jeevan

タグ(1)
0 件の賞賛
返信
1 解決策
740件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Jeevansagar 

S32K1xx devices have only one boot mode - from internal flash from address 0 (0x0 initial SP_main and 0x4 initial PC). There are no other options, so there are no boot pins.

Regards,

Lukas

 

 

 

 

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
741件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Jeevansagar 

S32K1xx devices have only one boot mode - from internal flash from address 0 (0x0 initial SP_main and 0x4 initial PC). There are no other options, so there are no boot pins.

Regards,

Lukas

 

 

 

 

 

 

 

0 件の賞賛
返信