Debugger mass erase

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugger mass erase

1,605件の閲覧回数
814420552
Contributor III

Hello,

   Debugger call mass erase command , is this command the same with erase all blocks unsecured command, thus erase command = erase all blocks unsecured command?

  if there is write protection, can erase all blocks unsecured command run ok?

  thanks in advance!

0 件の賞賛
返信
1 返信

1,569件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello Kui Wu,

The command used by the debugger depends on the debugger you're using, usually, in the Segger debugger first calls a normal to erase all but after detecting if there is secured the MCU there's a message mention this and confirmation if you want to unsecure the device. In this case, the debugger try to unsecure the device first writing to the FSEC[SEC].

Also if check the description from the Erase All Block/Erase All Blocks Unsecure you will notice that in the first one there is the following note:

The Erase All Blocks command aborts if any flash memory is protected by the FPROT register or FDPROT register or if the FlexRAM region is protected by the FEPROT register

This isn't the same for the unsecure, this will try to erase all the memory regardless of the protection the memory has.

Best Regards,

Alexis Andalon

0 件の賞賛
返信