Debugger mass erase

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugger mass erase

1,630 Views
814420552
Contributor III

Hello,

   Debugger call mass erase command , is this command the same with erase all blocks unsecured command, thus erase command = erase all blocks unsecured command?

  if there is write protection, can erase all blocks unsecured command run ok?

  thanks in advance!

0 Kudos
Reply
1 Reply

1,594 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello Kui Wu,

The command used by the debugger depends on the debugger you're using, usually, in the Segger debugger first calls a normal to erase all but after detecting if there is secured the MCU there's a message mention this and confirmation if you want to unsecure the device. In this case, the debugger try to unsecure the device first writing to the FSEC[SEC].

Also if check the description from the Erase All Block/Erase All Blocks Unsecure you will notice that in the first one there is the following note:

The Erase All Blocks command aborts if any flash memory is protected by the FPROT register or FDPROT register or if the FlexRAM region is protected by the FEPROT register

This isn't the same for the unsecure, this will try to erase all the memory regardless of the protection the memory has.

Best Regards,

Alexis Andalon

0 Kudos
Reply