Debugger Queries for S32K3X4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugger Queries for S32K3X4

ソリューションへジャンプ
2,087件の閲覧回数
ishoboiM
Contributor III

Hello, need to know that in the Emulators, probes section in the design resources section (attached photo below)

1. Whether the 5 products there have any feature comparison documents

2. As our main requirement need do the following, Can you let us know if

a. There is a Real time display of variable values in watch window.

b. We can modify variable values from the watch window.

c. We can export the data from a watch window to a csv/text/xlsx etc file

 

3. We want to pair it with S32K3xx device (specifically S32K344) and run our project

 

 
タグ(2)
0 件の賞賛
返信
1 解決策
2,047件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @ishoboiM,

1. There are no feature comparison documents, but you can look over at their respective pages to find some key differences:

Along with recommendations from our website below you could also take a look on third party providers’ website:

2.a. Yes. This is driver and debugger dependent, so I will use PEMicro as an example for the follow-up questions. You can use Real Time Variable from PEMicro, for example: Solved: How do I enable Live View for variables when debugging? - NXP Community.

You can also use something like FreeMaster for real time control: Solved: How to use FreeMaster and S32? - NXP Community.

2.b. See answer 2.a.

2.c. Yes. I believe SWO over PEMicro supports data export: Single Wire Output (SWO) support within S32 Design Studio, enabled by PEmicro's GDB Server - NXP Com....

3. This is fine. You can ask PEMicro (or whichever debugger solution you choose) themselves in their support page: PEMicro | Support.

Best regards,
Julián 

元の投稿で解決策を見る

2 返答(返信)
2,048件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @ishoboiM,

1. There are no feature comparison documents, but you can look over at their respective pages to find some key differences:

Along with recommendations from our website below you could also take a look on third party providers’ website:

2.a. Yes. This is driver and debugger dependent, so I will use PEMicro as an example for the follow-up questions. You can use Real Time Variable from PEMicro, for example: Solved: How do I enable Live View for variables when debugging? - NXP Community.

You can also use something like FreeMaster for real time control: Solved: How to use FreeMaster and S32? - NXP Community.

2.b. See answer 2.a.

2.c. Yes. I believe SWO over PEMicro supports data export: Single Wire Output (SWO) support within S32 Design Studio, enabled by PEmicro's GDB Server - NXP Com....

3. This is fine. You can ask PEMicro (or whichever debugger solution you choose) themselves in their support page: PEMicro | Support.

Best regards,
Julián 

1,801件の閲覧回数
ishoboiM
Contributor III
Thank you !