S32K Arm2.2 S32K116 cannot operate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K Arm2.2 S32K116 cannot operate

665 Views
mumumilmil
Contributor II

During debugging, the scope measures the real-time and signal output normally.
After debugging, remove the input Voltage from the power supply and apply power again, the MCU outputs nothing. Does CLOCK not come to life when power is re-entered? There is no sleep mode.

I used LPIT_inturrupt, FIRC sys clock. real-time works well.  plugged in. 

Is it associated to LPIT IRQHANDLER? 

0 Kudos
Reply
1 Reply

635 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Have you tested the lpit_periodic_interrupt_s32k116 project in S32K1 SDK 3.0.0?

Did you add "START_FROM_FLASH" Symbols in "Standard S32DS Assembler" by refer to the discussion in S32K188 runs with debugger, but not witout


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply