Debug S32K324 multi-core projects compiled with GHS using PE in S32DS.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug S32K324 multi-core projects compiled with GHS using PE in S32DS.

458 Views
yin2
Contributor I

Hi,

I want to consult about a relatively urgent issue:

How to configure settings to support multi-core debugging when debugging the S32K324 multi-core project via Processor Expert in S32DS?

Thanks!

0 Kudos
Reply
1 Reply

405 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hello @yin2,

Could you share which version of S32DS + RTD you are using? Since you've mentioned Processor Expert, then you may be using a legacy product. 

There are some useful documents in community:

The process is fairly simple; create 2 (or the number of cores needed) debug configurations and include them in a launch group. Keep in mind that the secondary core needs to be enabled, either by the debugger, or by the boot core.

You can also refer to the Whiteboard example package: Solved: S32K324 Multi-Core Example Project based on Whiteboard - NXP Community.

Best regards,
Julián

0 Kudos
Reply