Config tools version for S32K344 version mismatch?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Config tools version for S32K344 version mismatch?

ソリューションへジャンプ
2,764件の閲覧回数
stuartrubin
Contributor III

I have a S32K344 project developed by someone else. I have installed what I think is the latest version of the "MCUXpresso Config Tools", the IDE, etc., but the Config Tool will not open the file. There seems to be a version mismatch, but I cannot seem to get the right version of the tool(s). Can someone please provide a link to the right tool? Thank you.

version_not_supported.pngversion_not_supported.png

0 件の賞賛
返信
1 解決策
2,735件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

This project is created with old version S32K RTD. Please download the SW32K3_RTD_4.4_0.8.1_D2011_updatesite and install it by refer: HOWTO: S32 Design Studio - Offline Install of Extensions and Updates

Download SW32K3_RTD_4.4_0.8.1_D2011_updatesite.pngDownload SW32K3_RTD_4.4_0.8.1_D2011_updatesite.pngS32K3 Real Time Drivers 4.4 version 0.8.1.pngS32K3 Real Time Drivers 4.4 version 0.8.1.png

Then you will be able to open .mex file.

The SW32K3_RTD_4.4_0.8.1_D2011_updatesite  can be download from S32K3 Standard Software.

S32K3 Standard Software.pngS32K3 Standard Software.pngAutomotive SW - S32K3 Standard Software.pngAutomotive SW - S32K3 Standard Software.pngAutomotive SW - S32K3 - Real-Time Drivers for Cortex-M.pngAutomotive SW - S32K3 - Real-Time Drivers for Cortex-M.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,736件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

This project is created with old version S32K RTD. Please download the SW32K3_RTD_4.4_0.8.1_D2011_updatesite and install it by refer: HOWTO: S32 Design Studio - Offline Install of Extensions and Updates

Download SW32K3_RTD_4.4_0.8.1_D2011_updatesite.pngDownload SW32K3_RTD_4.4_0.8.1_D2011_updatesite.pngS32K3 Real Time Drivers 4.4 version 0.8.1.pngS32K3 Real Time Drivers 4.4 version 0.8.1.png

Then you will be able to open .mex file.

The SW32K3_RTD_4.4_0.8.1_D2011_updatesite  can be download from S32K3 Standard Software.

S32K3 Standard Software.pngS32K3 Standard Software.pngAutomotive SW - S32K3 Standard Software.pngAutomotive SW - S32K3 Standard Software.pngAutomotive SW - S32K3 - Real-Time Drivers for Cortex-M.pngAutomotive SW - S32K3 - Real-Time Drivers for Cortex-M.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信