CSEc secure boot and reset signal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CSEc secure boot and reset signal

ソリューションへジャンプ
1,651件の閲覧回数
snaku_lee
Contributor IV

Hi,

I have a question about the CSEc secure boot with sequential boot mode.

I want to measure the secure boot time from reset pin release to high, but I find there is no different while secure boot with different BOOT_SIZE?

So I guess when the secure boot is start to boot (i.e., the CSEc is computing the CMAC), the CPU core stay in reset state, and the reset pin also hold in low state, until CMAC compuing finish, am I right ?

Regards,

Snaku

タグ(1)
0 件の賞賛
返信
1 解決策
1,635件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Snaku,

You can find some execution time specs in AN5401.

danielmartynek_0-1629891972636.png

You are right, the reset_b pin is driven low as long as the core is in the reset state.

You can measure the time between a rising edge on the VDD power supply (after POR) and the rising edge on reset_b.

 

Regards,

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,636件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Snaku,

You can find some execution time specs in AN5401.

danielmartynek_0-1629891972636.png

You are right, the reset_b pin is driven low as long as the core is in the reset state.

You can measure the time between a rising edge on the VDD power supply (after POR) and the rising edge on reset_b.

 

Regards,

Daniel

0 件の賞賛
返信
1,617件の閲覧回数
snaku_lee
Contributor IV

Hi Daniel,

I got it, thanks for your support.

Snaku

0 件の賞賛
返信