CSEc secure boot and reset signal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CSEc secure boot and reset signal

Jump to solution
1,650 Views
snaku_lee
Contributor IV

Hi,

I have a question about the CSEc secure boot with sequential boot mode.

I want to measure the secure boot time from reset pin release to high, but I find there is no different while secure boot with different BOOT_SIZE?

So I guess when the secure boot is start to boot (i.e., the CSEc is computing the CMAC), the CPU core stay in reset state, and the reset pin also hold in low state, until CMAC compuing finish, am I right ?

Regards,

Snaku

Tags (1)
0 Kudos
Reply
1 Solution
1,634 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Snaku,

You can find some execution time specs in AN5401.

danielmartynek_0-1629891972636.png

You are right, the reset_b pin is driven low as long as the core is in the reset state.

You can measure the time between a rising edge on the VDD power supply (after POR) and the rising edge on reset_b.

 

Regards,

Daniel

View solution in original post

0 Kudos
Reply
2 Replies
1,635 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Snaku,

You can find some execution time specs in AN5401.

danielmartynek_0-1629891972636.png

You are right, the reset_b pin is driven low as long as the core is in the reset state.

You can measure the time between a rising edge on the VDD power supply (after POR) and the rising edge on reset_b.

 

Regards,

Daniel

0 Kudos
Reply
1,616 Views
snaku_lee
Contributor IV

Hi Daniel,

I got it, thanks for your support.

Snaku

0 Kudos
Reply