CAN baurate error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN baurate error

Jump to solution
3,591 Views
Andrew101
Contributor II

Hello everyone,

I have a problem with baurate in classic CAN in S32K3. I reuse an example code "lwip_baremetal_s32k344" and add FlexCAN. Although I configed in clock diagram tab, FlexCAN tab and the S32DS also return the approriate value is 1 MHz (see the pictures below for more details), when I measured CAN_TX by logic analyzer, I see the baurate was just around 400Khz. Does anyone have the same problem with me? Thanks for your help.

khanhhuy_0-1760150358678.pngkhanhhuy_1-1760150382392.png

khanhhuy_2-1760150458852.pngkhanhhuy_3-1760150484430.pngkhanhhuy_4-1760150505078.pngkhanhhuy_5-1760150580089.png

 

 

0 Kudos
Reply
1 Solution
3,435 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Andrew101

1. Regarding the CAN speed, as I mentioned, the CAN module configuration is correct, at 1M. You can check the ACK bit width; theoretically, it should be 1us. If it's not, check your MCU module.
(I can't run your code properly; I don't know why you're mixing MCAL and Drivers.)

https://community.nxp.com/t5/S32K-Knowledge-Base/RTD600-MCAL-amp-IP-S32K3X4EVB-T172-FlexCAN-Example-...


2. Regarding the LPI2C speed, your "Clock_Ip_ReferencePoints" configuration is incorrect; the clock is not the I2C module's clock.

View solution in original post

0 Kudos
Reply
7 Replies
3,543 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Andrew101

I don't see problem with your flexcan settings, could you please share your test picture and your project so that I can take time to reproduce your issues.

0 Kudos
Reply
3,539 Views
Andrew101
Contributor II

Of course,
Let me tell you again my problem. As you can see, in the configuration, the baurate is 1 Mbs, but when I measure on logic analyzer , the signal is just around 400 Kbs. Here are the picture and the whole project. I used on S32K344 EVB SCH 53148 Rev B board and s32ds 3.6.3, RTD 6.0.0

Andrew101_0-1760177024908.png

Andrew101_1-1760177276714.pngAndrew101_2-1760177292627.png

 

 

0 Kudos
Reply
3,470 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Andrew101

I think your measurement method is wrong.

You can use an oscilloscope to measure the minimum pulse width to calculate the bit rate.

Senlent_0-1760324467302.png

In your configuration:

Tq = 5 / 80mhz = 62.5ns

CAN bit time = (1 + 8+ 5 + 2) * 62.5 = 1000ns

Bit rate = 1 / 1000ns = 1000K

0 Kudos
Reply
3,468 Views
Andrew101
Contributor II

Can you explain more details, please? I don't really understand. The configuration in the project I gave you is for 1000K. But the logic analyzer just recorded 400K. Additionally, when I debugged deeply into register, I saw a register CTRL1 with the field "PRESDIV" is set 4 but not 0. I don't know if it is the reason?

0 Kudos
Reply
3,449 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Andrew101

The 400k you are currently displaying is not necessarily a single bit width, it may be multiple bits wide.

"when I debugged deeply into register, I saw a register CTRL1 with the field "PRESDIV" is set 4 but not 0"

In your configuration, the "Prescaler division factor is 5", so the PRESDIV should be 5-1 = 4, so it's correct.

0 Kudos
Reply
3,446 Views
Andrew101
Contributor II
Thanks for your answer. So back to my first question, I wonder that what's wrong with my project and config that CAN module can not reach at 1 Mbs? In the project, I reused the example code "lwip_baremetal_s32k344" and added some more peripherals. I don't know if it is the reason? Because I also tried with I2C and the problem is similar to CAN "Baurate of I2C I set is 400 Kbs but it just worked in 100 Kbs". I think I have some conflicts in the project but I can not find. If your project works well, please share with me!!!
0 Kudos
Reply
3,436 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Andrew101

1. Regarding the CAN speed, as I mentioned, the CAN module configuration is correct, at 1M. You can check the ACK bit width; theoretically, it should be 1us. If it's not, check your MCU module.
(I can't run your code properly; I don't know why you're mixing MCAL and Drivers.)

https://community.nxp.com/t5/S32K-Knowledge-Base/RTD600-MCAL-amp-IP-S32K3X4EVB-T172-FlexCAN-Example-...


2. Regarding the LPI2C speed, your "Clock_Ip_ReferencePoints" configuration is incorrect; the clock is not the I2C module's clock.

0 Kudos
Reply