CAN Current Source Capability

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CAN Current Source Capability

跳至解决方案
3,498 次查看
bjrajendra
Senior Contributor I

Hello all,

Currently I'm using S32K14x device. I would like to know the current sink capability of CAN RX Module.

I have seen I/O current sinking capability mentioned as 5mA when used as IO pin as shown below. Will it work same with CAN module of any baud rate.

pastedImage_1.png

Kindly help with suitable documents.

Raju

标签 (1)
0 项奖励
回复
1 解答
3,379 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Raju,

The RXD pin of the transceiver is an output, it is not an input.

As you can see below, there is a push-pull driver.

pastedImage_1.png

Specified as follows:

pastedImage_1.png

The RXD pin of the transceiver is connected to the CAN_RX pin of the MCU.

Where the CAN_RX pin is an input driven by the RXD driver.

pastedImage_3.png

Regards,

Daniel

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,378 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Raju,

The 5mA sink current applies for output pins only.

The CAN_RX function is an input, it is floating.

Regards,

Daniel 

0 项奖励
回复
3,378 次查看
bjrajendra
Senior Contributor I

Hi Daniel,

Thanks for the response.

In fact, we're planning to connect two TJA1050 transceiver IC to one CAN_TX & CAN_RX port. This transceiver IC has an RX terminal in the range of 10mA. Thus is it possible for CAN_RX port to deliver the same.

I may be misunderstood. Kindly guide in meeting the requirement.

Raju.

0 项奖励
回复
3,380 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Raju,

The RXD pin of the transceiver is an output, it is not an input.

As you can see below, there is a push-pull driver.

pastedImage_1.png

Specified as follows:

pastedImage_1.png

The RXD pin of the transceiver is connected to the CAN_RX pin of the MCU.

Where the CAN_RX pin is an input driven by the RXD driver.

pastedImage_3.png

Regards,

Daniel

0 项奖励
回复
3,378 次查看
bjrajendra
Senior Contributor I

Thanks Daniel for the support.

Raju.

0 项奖励
回复