Build Configuration (Folder/File Structure)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build Configuration (Folder/File Structure)

1,287 Views
Gama
Contributor II

Hi Community,

I'm facing trouble with the S32 Design Studio IDE. My project's "Components" folder/files aren't compiling or being included in the build, despite following the recommended directory structure. I've tried multiple such as:

"

  • Open your S32 Design Studio project.
  • Navigate to the "Project" menu and select "Properties."
  • In the properties dialog, go to "C/C++ General" > "Paths and Symbols."
  • Under the "Source Location" tab, ensure that the path to your "Components" folder is included. If not, add it.

"

But no success. Please find the attached image that shows the structure that I want I want to compile. 

微信图片_20230831180310.png微信图片_20230831180310.png

Could you please advise on how to configure the build settings correctly and ensure the "Components_A, B, and C" files are included? Any insights or steps would be appreciated.

thanks

 

#S32K #Build #components #build

0 Kudos
Reply
0 Replies