Board cannot be reached after full chip erase

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Board cannot be reached after full chip erase

7,725 次查看
nevozade
Contributor IV

Hello,

I am faced several times with this problem. After select the option 'Emergency Kinetis Device Recovery by Full Chip Erase' in the debug configurations(screenshot1), the board (S32K148) becomes unreachable. Trying to connect to the board with the debugger pops up an error window that I attached it as a screenshot. Then, the s32k148 becomes unconnected at all. I think this could be due to the option to completely erase, or manipulation of a memory area that shouldn't be deleted in some way that I don't know. I cannot even try to reset procedure because I did not have any connection to the board. Have you ever faced with this kind of problem? 

Best Regards.

 

PS: While searching for this problem, I found the question( https://community.nxp.com/t5/S32-Design-Studio/S32-Design-Studio-Flash-Mass-erase/m-p/826467 )that may be related to the my problem. Is there any solution to make the board connectable?

0 项奖励
回复
7 回复数

7,702 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi nevozade,

Please halt the MCU by P&E Recovery Utility, refer: Can't use PEmicro debugger with S32K118EVB2-Q048
Then you should be able to flash it again.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

7,695 次查看
nevozade
Contributor IV

Hi @Robin_Shen ,

I had tried this halting method before, but it does not work because the board never becomes halted even I cycle power many times. Briefly, Recovery Utility does not make halted our board. It can be caused because voltage level, any idea?

0 项奖励
回复

7,690 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

When you power the board by USB_MICRO(J24), does the board emulate BOOTLOADER or S32K148EVB?
If it was S32K148EVB, then OpenSDA is able to halt the MCU

If you want to cycle power the MCU when running Recovery Utility Tool:
1.connect pin1-2 J8(using P5V0=P5V0_V1SBC). connect pin2-3 J7(VDD=P5V0)
2.power the OpenSDA by USB_MICRO(J24)
3.cycle power the MCU by J9 external power supply

0 项奖励
回复

7,685 次查看
nevozade
Contributor IV

Hi @Robin_Shen ,

Actually thanks for your answers. However, I do not have S32K148 EVB, I just use the MCU, not evaluation board indeed. Thus, I cannot configurate/check any pins that you mentioned. It is a printed card that uses MCU of s32k148. Any solutions for this case?

Regards.

0 项奖励
回复

7,681 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Make sure the debug interface is correct. Check all VDD has powered.

4.2 JTAG and TRACE interface.png

Did you ever enable CSEc or secure MCU?

0 项奖励
回复

7,677 次查看
nevozade
Contributor IV

I cannot figure out what you referred with that image. Moreover, I have never enable security for this MCU before.

0 项奖励
回复

7,667 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

SWD_CLK recommend connected external pull-down resistor.
SWD_DIO recommend connected external pull-up resistor.
RESET recommend connect external pull-up resistor.

0 项奖励
回复