About flash clock maximum frequency.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About flash clock maximum frequency.

ソリューションへジャンプ
2,869件の閲覧回数
vienpeng
Contributor II
I'm using S32K146H, according to the reference manual, the flash clock maximum frequency is 26.67MHz (in RUN mode). My question: In actual project, is it recommended setting the maximum flash clock frequency ? My project is applied in the field of automobile and battery management system.
0 件の賞賛
返信
1 解決策
2,856件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

the microcontroller is designed to run continously at max frequencies, so there’s no need to decreased the flash clock. You can check Chapter 27: Clock Distrubution in the refefence manual:

https://www.nxp.com/webapp/Download?colCode=S32K1XXRM

There are examples of recommended configuration for individual modes.

Regards,

Lukas

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,857件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

the microcontroller is designed to run continously at max frequencies, so there’s no need to decreased the flash clock. You can check Chapter 27: Clock Distrubution in the refefence manual:

https://www.nxp.com/webapp/Download?colCode=S32K1XXRM

There are examples of recommended configuration for individual modes.

Regards,

Lukas

 

0 件の賞賛
返信
2,851件の閲覧回数
vienpeng
Contributor II
Thank you for your reply !
0 件の賞賛
返信