About flash clock maximum frequency.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About flash clock maximum frequency.

Jump to solution
2,920 Views
vienpeng
Contributor II
I'm using S32K146H, according to the reference manual, the flash clock maximum frequency is 26.67MHz (in RUN mode). My question: In actual project, is it recommended setting the maximum flash clock frequency ? My project is applied in the field of automobile and battery management system.
0 Kudos
Reply
1 Solution
2,907 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

the microcontroller is designed to run continously at max frequencies, so there’s no need to decreased the flash clock. You can check Chapter 27: Clock Distrubution in the refefence manual:

https://www.nxp.com/webapp/Download?colCode=S32K1XXRM

There are examples of recommended configuration for individual modes.

Regards,

Lukas

 

View solution in original post

0 Kudos
Reply
2 Replies
2,908 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

the microcontroller is designed to run continously at max frequencies, so there’s no need to decreased the flash clock. You can check Chapter 27: Clock Distrubution in the refefence manual:

https://www.nxp.com/webapp/Download?colCode=S32K1XXRM

There are examples of recommended configuration for individual modes.

Regards,

Lukas

 

0 Kudos
Reply
2,902 Views
vienpeng
Contributor II
Thank you for your reply !
0 Kudos
Reply