AN12218 UART bootloader problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AN12218 UART bootloader problem

ソリューションへジャンプ
2,323件の閲覧回数
wdong
Contributor III

I can update one program, when update another program, it seems that the EVB can update the program, but the program does not work, it has confused me a few days, please help me, thanks!

0 件の賞賛
返信
1 解決策
2,299件の閲覧回数
wdong
Contributor III

hello, I used the example code, and now i have solved the problem.

Because the .srec file is not 8byte aligned which created by the S32DS, one must change the file 8byte aligned like use hex-view software.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,305件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

 

Do you use your own project or example project?

Can you share the .srec file and linker file of the project which does not work?

You can check if the application is correctly loaded in the flash memory in the S32DS menu -> Window -> Show view -> Memory before the jump to the application.

Do you have S32K148?

 

Thank you.

Best regards,

Diana

0 件の賞賛
返信
2,300件の閲覧回数
wdong
Contributor III

hello, I used the example code, and now i have solved the problem.

Because the .srec file is not 8byte aligned which created by the S32DS, one must change the file 8byte aligned like use hex-view software.

0 件の賞賛
返信