AN12218 UART bootloader problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

AN12218 UART bootloader problem

跳至解决方案
2,322 次查看
wdong
Contributor III

I can update one program, when update another program, it seems that the EVB can update the program, but the program does not work, it has confused me a few days, please help me, thanks!

0 项奖励
回复
1 解答
2,298 次查看
wdong
Contributor III

hello, I used the example code, and now i have solved the problem.

Because the .srec file is not 8byte aligned which created by the S32DS, one must change the file 8byte aligned like use hex-view software.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,304 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

 

Do you use your own project or example project?

Can you share the .srec file and linker file of the project which does not work?

You can check if the application is correctly loaded in the flash memory in the S32DS menu -> Window -> Show view -> Memory before the jump to the application.

Do you have S32K148?

 

Thank you.

Best regards,

Diana

0 项奖励
回复
2,299 次查看
wdong
Contributor III

hello, I used the example code, and now i have solved the problem.

Because the .srec file is not 8byte aligned which created by the S32DS, one must change the file 8byte aligned like use hex-view software.

0 项奖励
回复