S32K Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K Knowledge Base

Labels

Discussions

Sort by:
This example project will show user how to use and configure the basic functionalities of WKPU + FlexCAN.   ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 (SCH-53148 REV B2) * MCU: S32K344 * IDE: S32DS3.5 & S32DS3.6 * SDK release: RTD 6.0.0 * Debugger: PE Micro * Target: internal_FLASH  ------------------------------------------------------------------------------ This example routine configures the FlexCAN0 instance for reception. Since RevB2 of the EVB was used for development, CAN TRXCVR used is TJA1443. TJA1443 is initialized in main code (CAN0_STB = 1 & CAN0_EN = 1). FlexCAN bitrate: Bitrate: 500 Kbps Sampling point: 81.25% Individual mask is set to 0x0, meaning all IDs are accepted. Main routine: Waits for SW5 to be pressed, or for FlexCAN interrupt. If SW5 is pressed, turns off green LED, disables FlexCAN and switches CORE_CLK to FIRC. It then configures both PTB19 (SW6) and PTA6 (CAN0_RX) for interrupt wakeups. If either SW6 is pressed or a CAN message is received (edge detect on PTA6), MCU wakes up and will wait for SW5 to be pressed again. FlexCAN is configured for INTERRUPT; If a CAN frame is received, bRxFlag is set to 1 inside the callback, blue LED is toggled, and an ACK frame is sent back. CAN communication can be tested either with another EVB, or with a PCAN analyzer connected to J32. PCAN-View log for dummy and ACK messages: This example is provided as is with no guarantees and no support.
View full article
*********************************************************************************** * Detailed Description: * The example locks * PFC PFCBLK2_SSPELOCK REG_PROT soft lock * and PFC REG_PROT hard lock. * ------------------------------------------------------------------------- * Test HW: : S32K344EVB-Q172 * MCU: : S32K344 * Project : RTD AUTOSAR 4.7 * Platform : CORTEXM * Peripheral : S32K3XX * Dependencies : none * * Autosar Version : 4.7.0 * Autosar Revision : ASR_REL_4_7_REV_0000 * SW Version : 5.0.0 * Build Version : S32K3_RTD_5_0_0_D2408_ASR_REL_4_7_REV_0000_20241002 ***********************************************************************************
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the  ADC_SAR and BCTU IP Driver for the S32K3xx MCU. The example uses the TWO PIT0 trigger to trigger BCTU conversion list to perform parallel conversions on ADC0/ADC1. Each Trigger has one LIST associated with it in the BCTU. Conversion result for EACH list is stored in individual FIFO of the BCTU. DMA will transfer the ADC conversion result. LIST-1 ADC channels are selected to be converted on each ADC:     LIST-2 ADC channels are selected to be converted on each ADC:--      Converted results from BCTU FIFO are moved by DMA into result array.  ADC channel S10 is connected to board's potentiometer. Result :--    ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ********************************************************************************
View full article
This page supports the NXP Tech Days training session AUT-T4984_Hands-On Workshop_Battery Management System Software Stack. The full installation pre-requisites are attached in the .zip bellow. Please follow closely BMS_SWInstalationGuide.pdf.
View full article
************************************************************************************************* * Detailed Description: * DCF record disables or enables POR_WDG depending on the POR_WDG_EN macro in main.c. * Find first available location in UTEST, by default, first available address is 0x1B000780 * * NOTE: There is a bug in this RTD version. * Change FLS_MAX_VIRTUAL_SECTOR to 272 in C40_Ip_Cfg.h * ------------------------------------------------------------------------------ * Test HW: : S32K312EVB-Q172 * MCU: : S32K312 * Project : RTD AUTOSAR 4.7 * Platform : CORTEXM * Peripheral : S32K3XX * Dependencies : none * * Autosar Version : 4.7.0 * Autosar Revision : ASR_REL_4_7_REV_0000 * Autosar Conf.Variant : * SW Version : 3.0.0 * Build Version : S32K3_RTD_3_0_0_D2303_ASR_REL_4_7_REV_0000_20230331 *************************************************************************************************
View full article
******************************************************************************* The purpose of this demo application is to present a usage of the EMIOS IP Driver in Polling mode for the S32K3xx MCU. The example use to :-- EMIOS-1 - ch-0  --> PTC24 --> Generate the PWM EMIOS-1 - ch-1  --> PTC25 --> is the ICU channel to measure the duty Pins used :--     This example is tested for IPWM mode .  :--       IPWM mode ,  ICU Driver User Manual :--   Result :-- Sometimes Compiling error comes, in Autogenerated RTD file.    Change the Header file name :--      ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************
View full article
The attached spreadsheet provides mapping between EIM and DCM faults for the S32K3x1, S32K3x2, S32K344, S32K324, and S32K314 devices. Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.
View full article
******************************************************************************** * Detailed Description: * The example updates th UART TX buffer for continuous transfer. * ---------------------------------------------------------------------- * Test HW: S32K344EVB-Q172 * MCU: S32K344, RTD 4.0.0 P24 * Debugger: S32DS_ARM_3.5 * Target: internal_FLASH ********************************************************************************
View full article
******************************************************************************************** * Test HW: S32K311 EVB-Q100 * MCU: S32K311 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************************** The purpose of this demo application is to enter the standby mode and waking up from sleep using the user button. =============== How this DEMO works ========== 1) once the image is flashed, the application starts running and BLUE LED blinks for every one second during RUN mode 2) Once SW5 in EVB is pressed, MCU enters the SLEEP mode and it turns off BLUE LED & PIT 3) To Wakeup: Press SW4 in EVB 4) Once it returns to normal mode, BLUE LED and PIT starts running. Used pins: ========= PTC11 -> SW5 -> EnterStandby PTA8 -> SW4 -> WakeupFromSleep PTB8 -> D12   -> Blue led  
View full article
This example project will show user how to use and configure the basic functionalities of WKPU + SIUL2.  ------------------------------------------------------------------------------ * Test HW: S32K312EVB-Q172 (SCH-50892 REV B) * MCU: S32K312 * IDE: S32DS v3.5 & S32DS v3.6.x * SDK release: RTD 6.0.0 * Debugger: PE Micro * Target: internal_FLASH  ------------------------------------------------------------------------------ This example routine configures the WKPU unit for a GPIO interrupt wake-up and defines a section in linker file for 32KB of Standby RAM. How to use Standby RAM? Modify the linker file to separatethe 32KBstandby RAM(0x2040 0000 ~0x2040 8000) from int_sram memory region, and place standby .bss and .data or .text sections into the new region as well as adjust the link address symbols for customized initialization during startup. Initialize the standby RAM only if it’s Power-On Reset. Use key word attribute to define the variable/function in relevant memory section. Counter variable is placed in standby ram section: __attribute__ ((section (".sram_standby_bss"))) volatile int RunStandbyCounter0 = 0; Linker file (.ld) must be modified accordingly. Standby sections and link address symbols must be placed: MEMORY { int_pflash : ORIGIN = 0x00400000, LENGTH = 0x001D4000 /* 2048KB - 176KB (sBAF + HSE)*/ int_dflash : ORIGIN = 0x10000000, LENGTH = 0x00020000 /* 128KB */ int_itcm : ORIGIN = 0x00000000, LENGTH = 0x00008000 /* 32KB */ int_dtcm : ORIGIN = 0x20000000, LENGTH = 0x0000F000 /* 60KB */ int_stack_dtcm : ORIGIN = 0x2000F000, LENGTH = 0x00001000 /* 4KB */ int_standbysram : ORIGIN = 0x20400000, LENGTH = 0X00000100 /* standby ram 256B*/ int_sram : ORIGIN = 0x20400100, LENGTH = 0x00007E00 /* 32KB - 0x100, needs to include int_sram_fls_rsv*/ int_sram_fls_rsv : ORIGIN = 0x20407F00, LENGTH = 0x00000100 int_sram_no_cacheable : ORIGIN = 0x20408000, LENGTH = 0x00007F00 /* 32KB , needs to include int_sram_results */ int_sram_results : ORIGIN = 0x2040FF00, LENGTH = 0x00000100 int_sram_shareable : ORIGIN = 0x20410000, LENGTH = 0x00008000 /* 32KB */ ram_rsvd2 : ORIGIN = 0x20418000, LENGTH = 0 /* End of SRAM */ } ... .sram_standby (NOLOAD): { . += ALIGN(4); *(.sram_standby_bss) } > int_standbysram ... __STANDBY_SRAM_START = ORIGIN(int_standbysram); __STANDBY_SRAM_SIZE = LENGTH(int_standbysram); Note 1: RAM ECC must be initialized only if it’s Power-on Reset. Note 2: CM7 CPU D-Cache MUST be disabled to use the Standby RAM area. Or set the standby RAM(0x2040 0000 ~0x2040 8000) as non-cacheable in MPU configuration. The routine waits for SW5 to be pressed, then turns off the green LED, and enters Wkpu_EnterStandby() function which: Disables D-Cache. Initializes RAM ECC (if reset was Power-on Reset). Adds +1 to the standby counter placed in Standby RAM. Switches core clock to FIRC. Initializes the WKPU instance. Configures WKPU42 (PTB19). Enters standby. If SW6 is pressed, MCU will perform a software reset through the Power_Ip_PerformReset() API. After wake-up, MCU resets and polls for SW5 to be pressed again. In this application, LPUART6 (connected to USB OpenSDA interface) is enabled and will show previous reset reason (external reset, power-on reset, wakeup, functional reset), as well as printing standby counter between resets/standby cycles. Connect a USB cable to J40, and open a Serial terminal on PC for the serial device with these settings:   9600 baud rate   No parity   One stop bit  No flow control   After either a SW reset, or a wake-up cycle, the standby counter will increase. If a destructive reset or Power-on Reset is asserted, the counter is reset.    This example is provided as is with no guarantees and no support.
View full article
This example project will show user how to use and configure the basic functionalities of WKPU + RTI (PIT0).  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 (SCH-53148 REV B2) * MCU: S32K344 * IDE: S32DS3.5 & S32DS3.6 * SDK release: RTD 6.0.0 * Debugger: PE Micro * Target: internal_FLASH  ------------------------------------------------------------------------------ This example routine configures the WKPU & PIT for wake-up. The PIT0 instance includes a dedicated RTI (Real Time Interrupt) timer that runs on a separate oscillator clock and can be used for system wakeup. A key feature of this is power saving with a separate input clock for the RTI timer. All other timers share a common core clock. Note: Only PIT_0 supports the RTI feature, and exists in the Standby domain. This example does not poll for a SW press to enter and configure standby; Instead, the main function directly enters the Wkpu_EnterStandby() function which: Switches core clock to FIRC. Initializes and configures WKPU instance and wake-up source 3 (RTI). Initializes and configures PIT0 and PIT0 CH0 as set in Config Tools view. If EN_RUN_ICYCL_DUTY macro is enabled, configures PIT1 for user code before going to standby. Once Pit1_Notification is entered, runFlag is set to FALSE. Turns off LED. Enables RTI channel interrupt (otherwise, MCU cannot be woken up). Finally, sets the timeout value (WKPU_ICYCL_DUTY_TIME macro) and enters standby. This showcases the basic configuration for template on a fast-scanning power saving routine (for example, wake-up, measure ADC, go back to sleep). Keep in mind that power saving depends on the frequency of wake-up events. If MCU spends more time in Run mode rather than in Standby mode, power consumption is affected. The transition time from Standby mode to Run mode is quick. If the MCU only spends 9ms in Run and 1ms in Standby, the average current of the system will be considerably higher than if the MCU was running only 1ms every 1 second. Refer to S32K3 Low Power Management AN and demos for further information. After the period defined with either WKPU_ICYCL_DUTY_TIME, MCU wakes up. After wake-up, MCU resets and the cycle repeats. This example is provided as is with no guarantees and no support.
View full article
This example project will show user how to use and configure the basic functionalities of WKPU + GPT RTC API.  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 (SCH-53148 REV B2) or S32K344MINI-EVB * MCU: S32K344 * IDE: S32DS3.5 & S32DS3.6 * SDK release: RTD 6.0.0 * Debugger: PE Micro * Target: internal_FLASH  ------------------------------------------------------------------------------ This example routine configures the WKPU & RTC units for wake-up. The RTC is present in always ON domain, hence available in RUN mode as well as in STANDBY mode.   The chip contains one instance of RTC (Real Time Clock) timer and API (Autonomous Periodic Interrupt) timer, where both can perform 32-bit comparisons. Both RTC and API timers can generate interrupts as well as wake-up from low power modes. The following figure highlights the path for RTC API wake-up. Please refer to Chapter 69.3.2 API functional description from the S32K3XX reference manual (Rev. 12) for further information.   The routine waits for SW5 to be pressed, then: Turns off the green LED Switches CORE_CLK to Option C - Boot Standby mode (CORE_CLK @ 24 MHz). Initializes the ICU driver. Configures RTC_API channel (WKPU0) Initializes GPT module. Starts timer and sets RTC_API_TIME. Enters standby. After the period defined, RTC API generates an interruption and MCU wakes up. After wake-up, MCU resets and polls for SW5 to be pressed again. The RTC API value can be changed with RTC_API_TIME definition. This example is provided as is with no guarantees and no support.
View full article
S32K1 vdd falling low voltage POR clear situation 1. Abstract This document primarily aims to explain the situation where the POR flag in the RCM_SSRS of the S32K1 chip is cleared, and to explain the setting status of the reset pin and the POR and LVD bits when VDD is powered down. This article is written because some customers, when using the RCM_SSRS reset flag to determine the corresponding RAM initialization conditions, have made incomplete considerations, leading to component failures in actual projects. They mistakenly believe that as long as the SSRS POR flag is not cleared by software writing a 1 after power-on, the POR bit will remain indefinitely. In reality, even after power-on, if subsequent power fluctuations cause VDD to drop to LVD/LVR and trigger a reset, the POR flag may still be automatically cleared by the chip.   2. Document content This article mainly categorizes VDD power-down scenarios into three main types: (1) VDD drops below the minimum LVR value but above VPOR, and then power is  back to normal VDD. In this case, reset flag POR=0 and LVD=1 in RCM_SSRS. (2) VDD drops below LVD, above LVR, and LVDRE=0. In this case, reset flag POR=1 and LVD=1 in RCM_SSRS. (3) VDD drops below LVD, above LVR, and LVDRE=1. In this case, reset flag POR=0 and LVD=1 in RCM_SSRS. The schematic diagram is as follows:   3. Test result on S32K116 board        
View full article
***************************************************************************** *Detailed Description: *This example will show you how to configure Wdg_fs23 Driver. *Sbc_fs23_InitDriver, Sbc_fs23_GoToInitState, Wdg_43_fs23_Init, Sbc_fs23_InitDevice initialize the Sbc device and external Wdg in SLOW MODE(This mode can e.g. be used during system startup/initialization phase). *Sbc_fs23_InitDevice release FS0B, according to the configuration in Sbc_fs23 WatchdogConfig tab: Release safety outputs after init *Sbc_fs23_TimeDelay delay for an amount of time, allow Gpt ISR to trigger watchdog externally. *Wdg_43_fs23_SetMode(WDGIF_FAST_MODE); switch Wdg operation mode to FAST MODE(This mode can e.g. be used during normal operations of the ECU). *Wdg_43_fs23_SetTriggerCondition(10000U); sets a new timeout value to 10 seconds, during which Wdg_fs23_Cbk_GptNotification0 continuously refresh the watchdog. *To demonstrate the watchdog timeout, Wdg_43_fs23_SetTriggerCondition was not called again to set a new timeout value, and Wdg_fs23_Cbk_GptNotification0 no longer refreshed the watchdog. *The watchdog error counter(WD_ERR_CNT) continues to increase reached its maximum value(WD_ERR_LIMIT), causing fault error counter(FLT_ERR_CNT) to increment by 1. *FS23 eventually enters fail-safe mode because FLT_ERR_CNT >= max. At this point, it was observed that LEDs V1 (D7), V2 (D8), and V3 (D9) of KITFS23SKTEVM were turned off. *The SPI data between FS23 and S32K311 are captured and attached to the project. *------------------------------------------------------------------------------ *Test HW: * S32K31XEVB-Q100 Board SCH-55131 REV A P32K311HV 0P98C * KITFS23SKTEVM Dev-kit SCH-53096 REV B2 MFS2320BMBB1EP * My S32K31XEVB-Q100 has an onboard PFS2320A0L1W1, but Step 13/14 of AN14041 mention that A0 devices are not supported, so S32K311 communicate with the FS23 on the KITFS23SKTEVM. *Connections: KITFS23SKTEVM | S32K31XEVB-Q100 ------------------------------|-------------------- SPI_CSB J28-2 | J12-5(PTB-17) SPI_MOSI J29-2 | J12-7(PTB-16) SPI_SCK J31-2 | J12-11(PTB-14) SPI_MISO J32-2 | J12.9(PTB-15) VCC J6-1 | J40-15 GND J6-2 | J40-13 - KITFS23SKTEVM: SW1 - position 2-3 , J30 - ON, J26 5-6 ON, J26 9-10 ON . - Connect KITFS23SKTEVM Dev-kit and S32K3 MCU via on-board Arduino headers. *SDK: * S32K3 RTD 4.0.0 (SW32K3_S32M27x_RTD_R21-11_4.0.0_D2311_DS_updatesite.zip) * FS23 RTD 1.0.0 (S32K3xx_SBC_FS23_R21-11_1.0.0_D2508_DesignStudio_updatesite.zip) *Debugger: S32DS 3.5.8, OpenSDA/ PEmicro Multilink Universal FX *Target: internal_FLASH *Reference: * AN14041 FS23 quick start guide (Rev. 2.0 — 23 January 2025) * AN14129 FS23 implementation and behaviors (Rev. 2.0 — 13 December 2024) * FS23, Safety System Basis Chip (SBC) with Power Management, CAN FD and LIN Transceivers Data Sheet (Rev. 8.0 — 30 June 2025) * RTD_SBC_FS23_UM.pdf C:\NXP\S32DS.3.5\S32DS\software\PlatformSDK_S32K3\SW32K3_FS23_R21-11_1.0.0_D2312\Sbc_fs23_TS_T40D34M10I0R0\doc * RTD_WDG_43_FS23_UM.pdf C:\NXP\S32DS.3.5\S32DS\software\PlatformSDK_S32K3\SW32K3_FS23_R21-11_1.0.0_D2312\Wdg_43_fs23_TS_T40D34M10I0R0\doc * AUTOSAR_SWS_WatchdogDriver.pdf https://www.autosar.org/fileadmin/standards/R21-11/CP/AUTOSAR_SWS_WatchdogDriver.pdf * This example is migrated from Wdg_fs23_example_HLD_S32K344. The method of migrating refers to the video "2.S32DS CT MCAL demo porting K344 to K312 based on RTD500": https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Tools-Part-How-to-port-RTD-s-existing-MCAL-demo-to-other/ta-p/1966315 *****************************************************************************
View full article
This example project will show user how to use and configure the basic functionalities of WKPU + SIUL2 (GPIO).  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 (SCH-53148 REV B2) * MCU: S32K344 * IDE: S32DS v3.5 & S32DS v3.6.x * SDK release: RTD 6.0.0 * Debugger: PE Micro * Target: internal_FLASH  ------------------------------------------------------------------------------ This example routine configures the WKPU unit for a GPIO interrupt wake-up. This is the simplest WKPU example. Pin PTB19 (WKPU42) is configured for wake-up.  The routine waits for SW5 to be pressed, then turns off the green LED, and enters Wkpu_EnterStandby() function which: Switches core clock to FIRC. Initializes the WKPU instance. Configures WKPU42 (PTB19). Enters standby (or fast standby). After pressing SW6, MCU wakes up, resets and polls for SW5 to be pressed again. This example is provided as is with no guarantees and no support.
View full article
* Detailed Description: * Updated the example lwip_FreeRTOS_s32K344 to enable pinging the lwIP stack * from the command window * *ping 192.168.0.209 * *Pinging 192.168.0.209 with 32 bytes of data: *Reply from 192.168.0.209: bytes=32 time=2ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 * *Ping statistics for 192.168.0.209: * Packets: Sent = 4, Received = 4, Lost = 0 (0% loss), *Approximate round trip times in milli-seconds: * Minimum = 1ms, Maximum = 2ms, Average = 1ms * * * EVB: * - All jumpers in default positions * * Configuration: * - Updated pin configuration * - Updated clock configuration * - IP address set to 192.168.0.209 and enabled UDP_ECHO, etc. * - Added DIO * * main.c * - Updated only the header * device.c * - No changes * test.c * - Commented out the code that shuts down the TCP/IP stack after * its predefined timeout * - Added LED task * * ----------------------------------------------------------------------------- * Test HW: S32K344MINI-EVB SCH-94921 REV B, 700-94921 REV B * MCU: S32K344 * Debugger: On Board * Target: internal_FLASH * EVB connection: EMAC <-> USB-to-Ethernet adapter <-> Laptop DELL, Windows 11
View full article
This example project will show user how to use and configure the basic functionalities of WKPU + RTC timeout.   ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 (SCH-53148 REV B2) * MCU: S32K344 * IDE: S32DS3.5 & S32DS3.6 * SDK release: RTD 6.0.0 * Debugger: PE Micro * Target: internal_FLASH  ------------------------------------------------------------------------------ This example routine configures the WKPU & RTC units for wake-up. The RTC is present in always ON domain, hence available in RUN mode as well as in STANDBY mode. The RTC can trigger a single wake-up event (timeout). When the RTC counter reaches a specific, pre-defined alarm time set by the user. RTC timeout is mapped as wake-up source 1. RTC0_CLK source is configured as SIRC_CLK, and SIRC_CLK must be enabled in standby mode. Chapter 69.3.1 RTC explains the functionality of the RTC timer. RTCVAL is updated at the point where no counter match is due as per the previous RTCVAL, the RTCF flag is set when the counter matches the new value. If there is a match when in the low-power mode, then the RTC first generates a wakeup request to force a wakeup to run mode, and then the RTCF flag is set. The routine waits for SW5 to be pressed, then turns off the green LED, and enters Wkpu_EnterStandby() function which: Switches CORE_CLK to FIRC. Initializes the WKPU instance. Configures WKPU1 & WKPU42 (PTB19). Initializes and enables interrupt for RTC. Loads the RTCVAL value to 5000ms.  Starts the counter. Enters standby (or fast standby). After the period defined with RTC_TIME or RTC_PERIOD_DELAY_MS(x) macros defined in Wkpu.h, MCU wakes up. After wake-up, MCU resets and polls for SW5 to be pressed again. This example is provided as is with no guarantees and no support.
View full article
This example project will show user how to use and configure the basic functionalities of ICU (WKPU) + CAN.   ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 (SCH-53148 REV B2) * MCU: S32K344 * IDE: S32DS3.5 & S32DS v3.6.x * SDK release: RTD 6.0.0 * Debugger: PE Micro * Target: internal_FLASH  ------------------------------------------------------------------------------ This project configures both Can_43_FLEXCAN and CanIf modules for CAN communication, along with the ICU (WKPU) module for wake-up. Transmission is done via POLLING, while reception is configured via INTERRUPT.  Tx MB is set to STD ID 123h. Acceptance mask is set to 0x0 (accept all IDs). CAN messages are sent using Can_43_FLEXCAN_Write() and received using the CanIf_RxIndication() callback. After CanIf_bRxFlag is set, an ACK message is sent back. If TJA1153 transceiver is used, macro TJA1153_EVB_TRCV must be used. If not, use TJA1043_EVB_TRCV for standard transceiver initialization (CAN0_STB & CAN0_EN pins set to HIGH).  FlexCAN bitrate is calculated with: CAN bit timing calculator sheet. CAN classic (non-FD) 24Mhz clock 500Kbps 81.3% Sample Point Main routine: Waits for SW5 to be pressed, or for FlexCAN Rx interrupt. If SW5 is pressed, turns off green LED, disables FlexCAN and switches CORE_CLK to FIRC. It then configures PTA6 (CAN0_RX) for wakeup. If a CAN message is received (edge detect on PTA6), MCU wakes up and will enter main routine again. If a CAN frame is received, MCU will wake-up and wait for SW5 to be pressed again. Note: The first CAN frame may not be fully received since there will be some time for the MCU to warm up from STANDBY mode back to RUN mode, so the application may need to ignore the first CAN frame. Note 2: In order to test this example, another CAN node must be connected to CAN0_OUT. This example is provided as is with no guarantees and no support.
View full article
The script performs secure‑recovery and mass‑erase initialization of locked S32K142 MCUs by keeping the device in system reset (PTA5 RESET_B held low) from the moment of power‑on. Before running the script, connect PTA5 (RESET_B) to VSS, power‑cycle the MCU, and start the script. The script first reads the MDM‑AP Status register to determine the MCU’s security and flash‑ready state, then prompts the user to initiate a mass‑erase operation through the MDM‑AP Control register. After the mass erase completes, the user is instructed to release RESET_B (remove PTA5 from VSS), after which the debugger re‑attaches and displays the flash configuration area at address 0x400. Finally, the script prompts whether the MCU should be reprogrammed from an ELF file, and if confirmed, programs flash, loads the project, and executes it.
View full article
**************************************************************************************************** * Detailed Description: * * SW triggered conversion of ADC0 internal channel 50 (ANAMUX_OUT). * ANAMUX is used for internal supply monitoring. * Supply to be monitored is configured using DCMRWF1 register. * * PIT is configured to generate interrupt each second then ADC conversion for selected supply is * SW started and measured result is printed to the UART interface * * ------------------------------------------------------------------------------------------------ * Test HW: S32K3x4EVB-T172 Rev B * MCU: S32K344_172HDQFP * IDE: S32DS 3.6.0 * RTD release: S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 6.0.0 * Debugger: Lauterbach, P&Emicro * Target: Internal_FLASH * Serial: 115200, 8N1 ***************************************************************************************************/ Terminal output
View full article