[S32K3 Tools Part] How to use VScode to compile EB MCAL project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[S32K3 Tools Part] How to use VScode to compile EB MCAL project

[S32K3 Tools Part] How to use VScode to compile EB MCAL project

[S32K3 Tools Part] How to use VScode to compile EB MCAL project


      For EB configured MCAL code, it is usually based on RTD and then compiled using the command line. When I first started learning, I always opened the relevant files directly to modify them, and then used the window cmd method to type commands. This method is very clumsy. Therefore, this article will show how to use VScode to open and compile a RTD4.0.0 S32K344 MCAL project. Of course, for MCAL EB projects, before compiling, you need to use the EB tool to open the configuration file of the corresponding project, and then close it after the project is generated.

1 VScode tool and configuration

VScode download link:

https://code.visualstudio.com/Download

After downloading, install it.

Here are some installation plug-ins I often use:

 1.png

Fig 1


2.png

Fig 2

You can search in extensions and install it directly.

2. Use VScode to compile the RTD MCAL project

This article takes RTD4.0.0, SW32K3_S32M27x_RTD_R21-11_4.0.0 as an example, and the platform is the official S32K344-EVB board. The code takes Dio_TS_T40D34M40I0R0 project as an example. In order not to affect the original routine, Dio_TS_T40D34M40I0R0 is copied and saved as Dio_TS_T40D34M40I0R0_vscode

2.1 Use EB tresos generate the configuration

Open EB tools, import the project in path:

C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_vscode\examples\EBT\S32K3XX\Dio_Example_S32K344\TresosProject

3.png

Fig 3

Double-click someId, then right-click. If you do not need to make custom configurations, just click generate project. Wait for the generation to complete without errors and close the EB IDE.

4.png

Fig 4

2.2 VScode  open project

   First open VScode and select the project path in open Folder:

C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_vscode\examples\EBT\S32K3XX\Dio_Example_S32K344

5.png

Fig 5

After opening, you can see that all the files in the path have been put in:


6.png

Fig 6

You can save the workspace so you don't need to open the folder every time.

File->Save workspace as, save to the path:

C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_vscode\examples\EBT\S32K3XX\Dio_Example_S32K344

 

2.3 Modify mk file

The project mk file needs to be modified to specify gcc, tresos paths, etc.

Modify points:project_parameters.mk

GCC_DIR = C:/NXP/S32DS.3.5_RTD400/S32DS/build_tools/gcc_v10.2/gcc-10.2-arm32-eabi
TRESOS_DIR = C:/EB/tresos_29_0_0
PLUGINS_DIR = C:/NXP/SW32K3_S32M27x_RTD_R21-11_4.0.0/eclipse/plugins

7.png

Fig 7

Modify points: check_build_params.mk

Delete

ifeq ("$(wildcard $(T32_DIR)/bin/windows/t32marm.exe)","")
    $(error Invalid path set to Trace32. \
    The provided path: from project_parameters.mk T32_DIR=$(T32_DIR) is invalid!)
Endif

8.png

Fig 8

Then save all files:File->save all

2.4 Compile the file

Terminal->New Terminal

Enter the following command:

>make generate
>make build

9.png

Fig 9

10.png

Fig 10

As you can see, after make build, an elf file has been generated in the out folder.

This elf file can be directly downloaded using two methods:

(1) S32DS empty project link to elf to download

(2) Lauderbach directly download elf file

 

2.5 debug the generated elf file

Since the S32K344-EVB has an onboard opensda tool, we directly use the S32DS empty project to link to the generated main.elf file to download and debug.

Create a new S32DS project, and the interface is PE Multilink, then directly change the elf file to main.elf in the debug configuration, and then put the previously generated elf file into the folder of the new S32DS project: 

\Debug_FLASH

11.png

Fig 11

Then, enter debug mode, the results are as follows:

12.png

Fig 12

As you can see, the chip has entered debug mode and can run successfully.

Running at full speed, you can see the onboard red light flashing, so at this point, VSCode has compiled the MCAL code and run successfully.

 

100%が役に立ったと言っています (1/1)
バージョン履歴
最終更新日:
‎10-03-2024 01:20 AM
更新者: