update code from CLI S32DS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

update code from CLI S32DS

ソリューションへジャンプ
2,647件の閲覧回数
cristianchacha
Contributor III

Hello I'm working with S32 Design Studio

 

My goal is build a project with CLI, actually I achieved import and build. Also I would like to update this code with a *.hex file.
I'm using SDK SJA1110, and I can update the code manually , using option load table from configuration file (in switchcore ), selecting file and push load button, after that I click in Updated code and generate code is updated.

Is possible realize these steps with CLI?.

 



0 件の賞賛
返信
1 解決策
2,593件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @cristianchacha , 

 

I am not sure about hex file, but you can use .elf file for sure. 

 

Please can you check this post if it helps: https://community.nxp.com/t5/S32-Design-Studio/s32k144-command-line-flash/m-p/805235

 

Please let us know if you are able to work forward.

 

Thank you.

 

Best regards. 

- Mehul Patel 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,627件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @cristianchacha , 

 

 

Please can you check this guide for reference guide

 

HOWTO: S32 Design Studio Command Line Interface:  https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-S32-Design-Studio-Command-Line-I...

 

Also you can use this as reference guide to understand although the guide is not for SJA1110

 

HOWTO: Command Line JTAG flash programming with S32 Debug Probe on S32G274A EVB 

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Command-Line-JTAG-flash-programm...

 

Please let us know if you have further question or specific requirement to SJA110 or related to the project. 

Thank you. Best regards. 

-Mehul Patel 

 

Please let us know if 

0 件の賞賛
返信
2,601件の閲覧回数
cristianchacha
Contributor III
Hello Mehul,

I reviewed HOWTO: S32 Design Studio Command Line Interface I found how to build, but my goal is import a hexfile to generate code and also buil the project.

Do you know is this feature is cover with CLI ??
0 件の賞賛
返信
2,594件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @cristianchacha , 

 

I am not sure about hex file, but you can use .elf file for sure. 

 

Please can you check this post if it helps: https://community.nxp.com/t5/S32-Design-Studio/s32k144-command-line-flash/m-p/805235

 

Please let us know if you are able to work forward.

 

Thank you.

 

Best regards. 

- Mehul Patel 

0 件の賞賛
返信