qspi running pfe_master project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

qspi running pfe_master project

81 Views
youke
Contributor III

Hi,NXP

I'm testing the S32G with rdb2 hardware, I haven't found a M core pfe master program that I can run on qspi, I just want the M core to be able to send out udp data via pfe just fine, is there a routine for that?

BR.

0 Kudos
Reply
1 Reply

39 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @youke 

Thanks for your post.

Since UDP is based on IP protocol, for sending UDP packet via PFE from M core's perspective, you need to combine the PFE driver and IP stack together(for example, LWIP),  I suggest referencing the demo that mentioned from example_application directory of the PFE MCAL for details.

chenyin_h_0-1759219361788.png

 

BR

Chenyin

 

 

BR
Chenyin

0 Kudos
Reply