enabling external EEPROM driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

enabling external EEPROM driver

1,581 次查看
sandeep3
Contributor I

Hello ,

i am using Gold Vip 1.11.0 package , for my custom build S32g399A board . where i am using ST M95M01-DWMN3

So i have integrated the EEPROM driver in the package but i am not able to enable the external driver reference container which is highlighted below, kindly let me know how to enable this container ,or any dependency related to this .
MicrosoftTeams-image.png

Thanks and Regards

Sandeep

标签 (1)
标记 (1)
0 项奖励
回复
4 回复数

1,568 次查看
sandeep3
Contributor I

Hi,

If Eep is not supported, then which driver should i use to access external EEPROM through SPI?

0 项奖励
回复

1,536 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

To access external EEPROM through SPI, we can recommend using the SPI driver available under the RTD, since it provides the basic SPI communication with S32G.

Please, let us know.

0 项奖励
回复

1,569 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We might be misunderstanding the overall inquiry. If so, we do apologize.

The Eep driver itself is used mainly for the uSDHC/eMMC communication under S32G, as told under the Eep Driver User Manual:

DanielAguirre_0-1720449747362.png

For which, we understand that it might not be enabled to interface with an external EEPROM under S32G, but for an SD or eMMC. More information can be found under the User Manual and Integration Manual available under the Eep plugin itself.

Please, let us know.

0 项奖励
回复

1,561 次查看
sandeep3
Contributor I
Hi,

If Eep is not supported, then which driver should i use to access external EEPROM through SPI?
0 项奖励
回复