enabling external EEPROM driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

enabling external EEPROM driver

1,582 Views
sandeep3
Contributor I

Hello ,

i am using Gold Vip 1.11.0 package , for my custom build S32g399A board . where i am using ST M95M01-DWMN3

So i have integrated the EEPROM driver in the package but i am not able to enable the external driver reference container which is highlighted below, kindly let me know how to enable this container ,or any dependency related to this .
MicrosoftTeams-image.png

Thanks and Regards

Sandeep

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

1,569 Views
sandeep3
Contributor I

Hi,

If Eep is not supported, then which driver should i use to access external EEPROM through SPI?

0 Kudos
Reply

1,537 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

To access external EEPROM through SPI, we can recommend using the SPI driver available under the RTD, since it provides the basic SPI communication with S32G.

Please, let us know.

0 Kudos
Reply

1,570 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We might be misunderstanding the overall inquiry. If so, we do apologize.

The Eep driver itself is used mainly for the uSDHC/eMMC communication under S32G, as told under the Eep Driver User Manual:

DanielAguirre_0-1720449747362.png

For which, we understand that it might not be enabled to interface with an external EEPROM under S32G, but for an SD or eMMC. More information can be found under the User Manual and Integration Manual available under the Eep plugin itself.

Please, let us know.

0 Kudos
Reply

1,562 Views
sandeep3
Contributor I
Hi,

If Eep is not supported, then which driver should i use to access external EEPROM through SPI?
0 Kudos
Reply