Yocto build error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Yocto build error

跳至解决方案
2,642 次查看
learnx
Contributor III

hardware:S32G399A

bsp version:bsp38.0

Reference documentation:S32G3_LinuxBSP_38.0_Quick_Start.pdf

 

My steps are as follows:

1. tools version

learnx_0-1708681124680.png

2. Getting the Yocto image,everything looks normal

learnx_1-1708681165244.png

3. Build Linux BSP, Report some error

a. sudo apt update

b. ./sources/meta-alb/scripts/host-prepare.sh

learnx_3-1708682715821.png

c. source nxp-setup-alb.sh -m s32g399aevb3

learnx_4-1708682738790.png

d.bitbake fsl-image-auto, error

learnx_2-1708682634808.png

learnx_5-1708682814727.png

 

The previous preparations seem to be fine, but the build fails. How can I troubleshoot the problem?

0 项奖励
回复
1 解答
2,641 次查看
learnx
Contributor III
0 项奖励
回复
4 回复数
2,504 次查看
chenyin_h
NXP Employee
NXP Employee

Really glad to hear that, you are welcome.

 

Best Regards

Chenyin

0 项奖励
回复
2,610 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @learnx

Thanks for the question

From the BSP user manual, all operating steps are validated on ubuntu20.04 LTS, may I know if you are using the same version Ubuntu as the building host? I also tried the same building locally but do not find any issues.

Seems it is a connection problem, would you please help to check if you have connecting issue to the github? then try another build.

 

Best Regards

Chenyin

 

0 项奖励
回复
2,517 次查看
learnx
Contributor III

My local git configuration problem has been solved, thank you

0 项奖励
回复
2,642 次查看
learnx
Contributor III

error log

learnx_0-1708683245992.png

 

0 项奖励
回复