Yocto build error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,817件の閲覧回数
learnx
Contributor III

hardware:S32G399A

bsp version:bsp38.0

Reference documentation:S32G3_LinuxBSP_38.0_Quick_Start.pdf

 

My steps are as follows:

1. tools version

learnx_0-1708681124680.pnglearnx_0-1708681124680.png

2. Getting the Yocto image,everything looks normal

learnx_1-1708681165244.pnglearnx_1-1708681165244.png

3. Build Linux BSP, Report some error

a. sudo apt update

b. ./sources/meta-alb/scripts/host-prepare.sh

learnx_3-1708682715821.pnglearnx_3-1708682715821.png

c. source nxp-setup-alb.sh -m s32g399aevb3

learnx_4-1708682738790.pnglearnx_4-1708682738790.png

d.bitbake fsl-image-auto, error

learnx_2-1708682634808.pnglearnx_2-1708682634808.png

learnx_5-1708682814727.pnglearnx_5-1708682814727.png

 

The previous preparations seem to be fine, but the build fails. How can I troubleshoot the problem?

0 件の賞賛
返信
1 解決策
2,816件の閲覧回数
learnx
Contributor III

error log

learnx_0-1708683245992.pnglearnx_0-1708683245992.png

 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,679件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Really glad to hear that, you are welcome.

 

Best Regards

Chenyin

0 件の賞賛
返信
2,785件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @learnx

Thanks for the question

From the BSP user manual, all operating steps are validated on ubuntu20.04 LTS, may I know if you are using the same version Ubuntu as the building host? I also tried the same building locally but do not find any issues.

Seems it is a connection problem, would you please help to check if you have connecting issue to the github? then try another build.

 

Best Regards

Chenyin

 

0 件の賞賛
返信
2,692件の閲覧回数
learnx
Contributor III

My local git configuration problem has been solved, thank you

0 件の賞賛
返信
2,817件の閲覧回数
learnx
Contributor III

error log

learnx_0-1708683245992.pnglearnx_0-1708683245992.png

 

0 件の賞賛
返信