Yocto Linux BSP Image not Booting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto Linux BSP Image not Booting

1,236件の閲覧回数
Sri_5600
Contributor I

Hi Team,

We created a Yocto Linux BSP 33.0 image and attempted to boot the s32g274ardb2 board from an SD card. However, we discovered that only these logs are generated during bootup. Please see the log below and let us know how we can fix it with Complete logs. Thank you ahead of time.

NOTICE:  Reset status: Power-On Reset  
NOTICE:  BL2: v2.5(release):bsp33.0.hf1-2.5-dirty
NOTICE:  BL2: Built : 13:14:01, Aug 11 2022
NOTICE:  BL2: Booting BL31   
 
Error Image.jpg
0 件の賞賛
返信
2 返答(返信)

1,208件の閲覧回数
gmocanu
NXP Employee
NXP Employee

Hello,

It seems like you are using the Realtime Bootloader integrated in GoldVIP to bring up the system - have you updated the Bootloader configuration? How did you build the Linux image?

Please be aware that the boot process employed in GoldVIP is different than the one adopted in Linux BSP - more details at https://community.nxp.com/t5/S32G/what-s-the-differences-between-GoldVIP-s-ATF-and-bsp32-s-ATF/m-p/1...

Thank you,
George

1,196件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

g

タグ(1)
0 件の賞賛
返信