Safety Sboot CMU FC testing - Not enabling CMU_FC check before initiating CMU enabled tests

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Safety Sboot CMU FC testing - Not enabling CMU_FC check before initiating CMU enabled tests

489件の閲覧回数
Irshad2225
Contributor III

Hi, 

While CMU FC testing in sboot_cmuEnabledTests(), the CMU FC Check shall be True.

For the respective CMU FCs, the pCmu->GCR.B.FCE is not enabled in the plugins while running sboot stand-alone. Should it be done manually? or any prerequisites required?

Working when manually enabling pCmu->GCR.B.FCE.

cmu_fc.png
Regards,
Irshad

ラベル(1)
タグ(4)
0 件の賞賛
返信
2 返答(返信)

407件の閲覧回数
Joey_z
NXP Employee
NXP Employee

hi,Irshad2225

Thank you for your information.

You can try to use the sCheck_CmuFc_PrepareRun() function, this function has to enable the frequency check(pCmu->GCR.B.FCE = 1U;).

Hope it can help you.

BR

Joey

0 件の賞賛
返信

444件の閲覧回数
Joey_z
NXP Employee
NXP Employee

hi,Irshad2225

Thank you for contacting us.

I'm checking the answer for you and will reply to you as soon as there is a result.

BR

Joey

0 件の賞賛
返信