Safety Sboot CMU FC testing - Not enabling CMU_FC check before initiating CMU enabled tests

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Safety Sboot CMU FC testing - Not enabling CMU_FC check before initiating CMU enabled tests

410 次查看
Irshad2225
Contributor III

Hi, 

While CMU FC testing in sboot_cmuEnabledTests(), the CMU FC Check shall be True.

For the respective CMU FCs, the pCmu->GCR.B.FCE is not enabled in the plugins while running sboot stand-alone. Should it be done manually? or any prerequisites required?

Working when manually enabling pCmu->GCR.B.FCE.

cmu_fc.png
Regards,
Irshad

标签 (1)
标记 (4)
0 项奖励
回复
2 回复数

328 次查看
Joey_z
NXP Employee
NXP Employee

hi,Irshad2225

Thank you for your information.

You can try to use the sCheck_CmuFc_PrepareRun() function, this function has to enable the frequency check(pCmu->GCR.B.FCE = 1U;).

Hope it can help you.

BR

Joey

0 项奖励
回复

365 次查看
Joey_z
NXP Employee
NXP Employee

hi,Irshad2225

Thank you for contacting us.

I'm checking the answer for you and will reply to you as soon as there is a result.

BR

Joey

0 项奖励
回复