S32G399A IPCF

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,473件の閲覧回数
liujian1
Contributor I

HI, NXP:

         I have now successfully established the complete link using the IPC example project. However, I encountered some issues during the APP development and need some assistance.
After the IPCF runs, no dev device is created. The example project also directly uses addresses for interaction. Is there any way to create the IPC as a dev device? The application program handles data interaction through write and read.
タグ(2)
0 件の賞賛
返信
1 解決策
1,453件の閲覧回数
Joey_z
NXP Employee
NXP Employee

hi,liujian1

Thank you for contacting us.

You can consider using the ipc-shm-cdev.ko module and sample_user demo. It can be used as a reference.

Joey_z_0-1746615595860.png

Hope it can help you.

BR

Joey

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,454件の閲覧回数
Joey_z
NXP Employee
NXP Employee

hi,liujian1

Thank you for contacting us.

You can consider using the ipc-shm-cdev.ko module and sample_user demo. It can be used as a reference.

Joey_z_0-1746615595860.png

Hope it can help you.

BR

Joey

0 件の賞賛
返信