S32G399A IPCF

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G399A IPCF

Jump to solution
1,524 Views
liujian1
Contributor I

HI, NXP:

         I have now successfully established the complete link using the IPC example project. However, I encountered some issues during the APP development and need some assistance.
After the IPCF runs, no dev device is created. The example project also directly uses addresses for interaction. Is there any way to create the IPC as a dev device? The application program handles data interaction through write and read.
Tags (2)
0 Kudos
Reply
1 Solution
1,504 Views
Joey_z
NXP Employee
NXP Employee

hi,liujian1

Thank you for contacting us.

You can consider using the ipc-shm-cdev.ko module and sample_user demo. It can be used as a reference.

Joey_z_0-1746615595860.png

Hope it can help you.

BR

Joey

View solution in original post

0 Kudos
Reply
1 Reply
1,505 Views
Joey_z
NXP Employee
NXP Employee

hi,liujian1

Thank you for contacting us.

You can consider using the ipc-shm-cdev.ko module and sample_user demo. It can be used as a reference.

Joey_z_0-1746615595860.png

Hope it can help you.

BR

Joey

0 Kudos
Reply