S32G399A IPCF

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32G399A IPCF

跳至解决方案
1,474 次查看
liujian1
Contributor I

HI, NXP:

         I have now successfully established the complete link using the IPC example project. However, I encountered some issues during the APP development and need some assistance.
After the IPCF runs, no dev device is created. The example project also directly uses addresses for interaction. Is there any way to create the IPC as a dev device? The application program handles data interaction through write and read.
标记 (2)
0 项奖励
回复
1 解答
1,454 次查看
Joey_z
NXP Employee
NXP Employee

hi,liujian1

Thank you for contacting us.

You can consider using the ipc-shm-cdev.ko module and sample_user demo. It can be used as a reference.

Joey_z_0-1746615595860.png

Hope it can help you.

BR

Joey

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,455 次查看
Joey_z
NXP Employee
NXP Employee

hi,liujian1

Thank you for contacting us.

You can consider using the ipc-shm-cdev.ko module and sample_user demo. It can be used as a reference.

Joey_z_0-1746615595860.png

Hope it can help you.

BR

Joey

0 项奖励
回复