- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I am working on bringing up the M7 UART port on a Goldbox. I created the UART example "Uart_Example_S32G399_M7" from the RTD AUTOSAR 4.4 in S32DS 3.5. I tried using both the original linker_ram.ld file and a modified one from the software enablement guide, but I am not seeing any output on the console.
Here are the details:
Console Settings (PuTTY):
- Baud rate: 9600
- Data bits: 8
- Parity: None
Changes Made:
- Applied the modified .ld SRAM configuration as per the software enablement guide.
- Made corresponding changes in the IVT.
Interestingly, using the modified .ld SRAM configuration, I was able to get the LED example working, but I am unsure why the UART example does not produce any output.
Could someone help me identify what might be going wrong?
Here are the IVT setting, original and modified .ld SRAM configurations for reference:
int_sram : ORIGIN = 0x34000000, LENGTH = 0x00500000 /* 5MB */
int_sram_no_cacheable : ORIGIN = 0x34500000, LENGTH = 0x00100000 /* 1MB, needs to include int_results */
ram_rsvd2 : ORIGIN = 0x34600000, LENGTH = 0 /* End of SRAM */
int_sram : ORIGIN = 0x34004000, LENGTH = 0x00400000 /* 4MB */
int_sram_stack_c0 : ORIGIN = 0x34404000, LENGTH = 0x00002000 /* 8KB */
int_sram_stack_c1 : ORIGIN = 0x34406000, LENGTH = 0x00002000 /* 8KB */
int_sram_stack_c2 : ORIGIN = 0x34408000, LENGTH = 0x00002000 /* 8KB */
int_sram_stack_c3 : ORIGIN = 0x3440A000, LENGTH = 0x00002000 /* 8KB */
int_sram_no_cacheable : ORIGIN = 0x34500000, LENGTH = 0x00100000 /* 1MB, needs to include int_results */
ram_rsvd2 : ORIGIN = 0x34600000, LENGTH = 0x00DFFFFF /* End of SRAM */
Thanks,
XD
Solved! Go to Solution.

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello, @XD
I apologize for the delay.
Just checked this version example from my side with the default ld files, seems no issue found for the test.
The following tips for your reference.
- Check the peripheral perspective, add the following drivers
- From the IntCtrl_Ip view, add the interrupt 83 for the example, since this example is working with interrupts
Then generate code and recompile for the project.
Hope it helps
Best Regards
Chenyin

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello, @XD
I apologize for the delay.
Just checked this version example from my side with the default ld files, seems no issue found for the test.
The following tips for your reference.
- Check the peripheral perspective, add the following drivers
- From the IntCtrl_Ip view, add the interrupt 83 for the example, since this example is working with interrupts
Then generate code and recompile for the project.
Hope it helps
Best Regards
Chenyin