S32G start error with a wrong RSTB signal ,cause VR5510 FS0B assert

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32G start error with a wrong RSTB signal ,cause VR5510 FS0B assert

973 次查看
GuoGuo
Contributor II

      When we start code from norflash  use QuadSPI boot ,  in our own boad .There is always a wrong RESB like the picture attatched below .The code  running well ,but The VR5510 can‘t get in stadby mode,VR5510 FSM_STATES always is ASSERT_FS0B! Which may cause that ,how can we solve this problem to release VR5510 FS0B.The VR5510 error count is always 2 .The register shows us it can't find a EXT reset signal.

GuoGuo_0-1667208677001.png

GuoGuo_1-1667208867240.pngGuoGuo_2-1667208890739.png

 

 

标记 (1)
0 项奖励
回复
1 回复

931 次查看
MayanksPatel
NXP Employee
NXP Employee

Hi @GuoGuo,

Thank you for reaching out to us.

Will you share more details when you are facing the issue on boot time or on stand-by condition?

Also, please describe the impact of the issue. Is it not properly booting or having issues with Stand-by?

 

Thanks,

Mayank s Patel

0 项奖励
回复