S32G set lockstep

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G set lockstep

2,102件の閲覧回数
liuchi
Contributor III

Hi All:
How to enable the lockstep mode of the S32G during the boot stage? Are there any detailed references?
I only saw the description of the lockstep register in the manual, which needs to be configured in the M7 core. Can it be configured through DCB?
Thinks!

タグ(2)
0 件の賞賛
返信
5 返答(返信)

2,083件の閲覧回数
Joey_z
NXP Employee
NXP Employee

hi,liuchi

Thank you for contacting us.

Are you using the S32G2 or S32G3?

BR

Joey

0 件の賞賛
返信

2,064件の閲覧回数
liuchi
Contributor III

Both s32G3 and S32G2 are in use,They are different about lockstep?

0 件の賞賛
返信

2,064件の閲覧回数
liuchi
Contributor III
Both s32G3 and S32G2 are in use
0 件の賞賛
返信

2,031件の閲覧回数
Joey_z
NXP Employee
NXP Employee

hi,liuchi

Thank you for your reply.

You can refer to the BSP User Manual and find more lockstep operation.

Joey_z_0-1747706645729.png

Hope it can help you.

BR

Joey

 

0 件の賞賛
返信

1,896件の閲覧回数
liuchi
Contributor III

Think you

0 件の賞賛
返信