S32G set lockstep

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G set lockstep

2,103 Views
liuchi
Contributor III

Hi All:
How to enable the lockstep mode of the S32G during the boot stage? Are there any detailed references?
I only saw the description of the lockstep register in the manual, which needs to be configured in the M7 core. Can it be configured through DCB?
Thinks!

Tags (2)
0 Kudos
Reply
5 Replies

2,084 Views
Joey_z
NXP Employee
NXP Employee

hi,liuchi

Thank you for contacting us.

Are you using the S32G2 or S32G3?

BR

Joey

0 Kudos
Reply

2,065 Views
liuchi
Contributor III

Both s32G3 and S32G2 are in use,They are different about lockstep?

0 Kudos
Reply

2,065 Views
liuchi
Contributor III
Both s32G3 and S32G2 are in use
0 Kudos
Reply

2,032 Views
Joey_z
NXP Employee
NXP Employee

hi,liuchi

Thank you for your reply.

You can refer to the BSP User Manual and find more lockstep operation.

Joey_z_0-1747706645729.png

Hope it can help you.

BR

Joey

 

0 Kudos
Reply

1,897 Views
liuchi
Contributor III

Think you

0 Kudos
Reply