S32G-VNP-RDB2 Lauterbach

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G-VNP-RDB2 Lauterbach

15,026 Views
NP1
Contributor III

Can someone tell which debugger will support in S32G-VNP-RDB2 board. Will Debugger LA-3000 will support in this board? 

 

0 Kudos
Reply
14 Replies

14,966 Views
NP1
Contributor III

We are trying load  LwIP example on S32G-VNP-RDB2 board and the Lauterbach we use is LA-3500 (debug module) with LA-3255 and LA-7844x (debugger for ARM A/R [arm8/9] with extension to cortex M series).

NP1_0-1681721849318.pngNP1_0-1681721849318.png

But we were getting the above error (bus error at  address 0x34500000).  Is there any restriction to write to this memory location? or ho to resolve this error

0 Kudos
Reply

14,955 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We assume you are trying to run the LWIP example that comes with the TCP/IP stack (non PFE). If so, have you installed HSE-FW? This is a requisite for the example to be able to run. There is a workaround talked in the following thread which explains the modifications needed if HSE-FW is not available:

Solved: Ethernet Bring up - NXP Community

As for the memory space, we see that it is defined on the linker file, which means it should be available:

DanielAguirre_0-1681761369931.pngDanielAguirre_0-1681761369931.png

Is this same problem happening with a blink example?

Please, let us know.

0 Kudos
Reply

14,946 Views
NP1
Contributor III
Yes it is the LWIP example that comes with the TCP/IP stack . Same is happening with LED blink one as well.
0 Kudos
Reply

14,926 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback.

Which *.cmm files are you using for your setup?

Please, let us know.

0 Kudos
Reply

14,899 Views
NP1
Contributor III

I have attached the same S32G2_load.txt (note: just changed the extension for uploading purpose) 

0 Kudos
Reply

14,860 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We have received the following update from our internal team:

"0x34500000 is the start address of non-cacheable memory in LwIP example, the customer used the incorrect trace script which caused this issue, the script to be used should be "s32g2_connect_m7_0". This script can found in T32\demo\arm_obsolete\hardware\s32g2\scripts"

If you cannot find this script, help us opening a ticket on the NXP online services, for us to be able to share more information on regards of this topic.

Please, let us know.

0 Kudos
Reply

14,713 Views
NP1
Contributor III
When I open s32g2_connect_m7_0.cmm script , we were getting stopped at vector catch error . ST:3400020 [
\\User\Global\_ResetVector ]
0 Kudos
Reply

14,708 Views
rweiss
Contributor V

Hi @NP1,

perfect, the core is now stopped right at it's reset vector. This is the expected result after runing this script.

Regards,
Reinhard

0 Kudos
Reply

14,702 Views
NP1
Contributor III
Okay. So after that I just need to load the elf right ?
0 Kudos
Reply

14,836 Views
rweiss
Contributor V

demo\arm_obsolete\hardware\s32g2\scripts is not part of the official TRACE32 installation. The actual path is demo\arm\hardware\s32g2\scripts

Regards,
Reinhard

0 Kudos
Reply

14,879 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback. We will ask the internal team if they have seen this behavior before.

Please, let us know.

0 Kudos
Reply

14,992 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For S32G, we have the following information on regards of Lauterbach tools:

DanielAguirre_0-1681491145044.pngDanielAguirre_0-1681491145044.png

DanielAguirre_1-1681491167579.pngDanielAguirre_1-1681491167579.png

For which we are not seeing the specific P/N you are mentioning.

Still, we recommend sending the inquiry to Lauterbach support itself, since they will provide more information on regards of their platform.

Please, let us know.

0 Kudos
Reply

14,844 Views
rweiss
Contributor V

Hi @Daniel-Aguirre,

the debugger setup is suitable for S32G. Some order numbers changed since these pages were created.The pages show the recommended configuration at that time, but usually older hardware will also support newer processors, by updating the debugger software.

Best regards
Reinhard

15,006 Views
viswa_kondapall
Contributor IV

Hi ,

I think any licensed one will support. But u need .cmm scripts to debug. Those are available with most of the nxp SW bundles. Most of the projects has this .cmm files. goldvip binaries etc. folders search. please let me know. not able to find.

regards,

Viswa.

0 Kudos
Reply