S32G RDB2 multicore boot hang in bsp41

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32G RDB2 multicore boot hang in bsp41

跳至解决方案
8,120 次查看
Allen_Cheng
Contributor II

Hi NXP team,

 

I try to setup a multicores environment with A53 and M7 following AN13750 official document.

I found a boot issue in bsp41 and I also use bsp42 to clarify.

But BSP42 can bootup to Linux kernel successfully.

BSP41 will always hang in

bootloader 0x2 Application 1 image fragment 0 loaded from QSPI.
bootloader 0x2 Application M7_0 was loaded.

I add these two versions log in attachment.

Could you please help to clarify this issue?

Thanks.

 

SW:

Integration_Reference_Examples_S32G2_2023_06

EB 27.1

RTD 4.4_4.0.0_P05_HF01

HSE_FW S32G2XX_0_1_0_16

 

 

 

 

0 项奖励
回复
1 解答
7,581 次查看
Joey_z
NXP Employee
NXP Employee

HI,Allen_Cheng

After investigation, this is a known issue as described in ALB-11457, and it has been resolved in Linux BSP42. The root cause lies in the bootloader de-initializes (in SysDal) the peripheral clocks before starting the applications, but s32_io_setup() is called without any prior initialization of the SDHC clocks from ATF. The description is shown in the BSP42 release note:

Joey_z_0-1736506523488.png

The easiest solution to fix this issue is recommending use BSP>=42. If continue working with BSP41, you can refer to these public commits to modify ATF code.

Hope it can help you.

BR

Joey

在原帖中查看解决方案

0 项奖励
回复
13 回复数
8,097 次查看
Joey_z
NXP Employee
NXP Employee

hi,Allen_Cheng

Did you change the ATF Load address and Entry point in the Bootloader? As shown in the following figure, the corresponding address is different for different versions of BSP.

Joey_z_0-1733455728747.png

Also, you need to check that no SRAM image loading and running addresses of M7 and fip are conflicting

BR

Joey

 

0 项奖励
回复
8,083 次查看
Allen_Cheng
Contributor II
Hi Joey,

The ATF load address are the same in bsp41/bsp42.
Entry point are 0x34700000.
Thanks.

Allen
0 项奖励
回复
7,971 次查看
Joey_z
NXP Employee
NXP Employee

hi,Allen_Cheng

Thank you for your reply.

Your BSP41 print message attachment shows that BL2 should not be started, check to see if the fip.bin of BSP41 was loaded correctly during your compliance with AN13750.

In addition, in order to provide better support, whether you can provide your blob.bin, I will test this problem for you as soon as possible.

BR

Joey

0 项奖励
回复
7,946 次查看
Allen_Cheng
Contributor II

Hi Joey,

 

Attachment is my blob.bin.

Thanks.

0 项奖励
回复
7,914 次查看
Joey_z
NXP Employee
NXP Employee

hi,Allen_Cheng

I have received your blob.bin and have repeated your problem and will solve it as soon as possible.
In addition, I found that BSP41 can be started using your blob.bin and BSP42's fip.bin, you can try it, I suspect that this may be caused by some initialization conflict between the ATF in BSP41 and the Bootloader used, this needs further testing.

BR

Joey

0 项奖励
回复
7,901 次查看
Allen_Cheng
Contributor II

Hi Joey,

 

I used the blob.bin and BSP42's fip.bin with BSP41's sdcard(official image+BSP41's fip.s32).

It can bootup to linux successfully.

So the result means the first question BL2 can't start in BSP41 may have certain issue?  

 

Another confusion:

If the ATF Load address and others condition are the same in BSP41 and BSP42, the blob.bin need to rebuild again? or they can use the same blob.bin?

 

Thanks!

 

Allen

0 项奖励
回复
7,812 次查看
Joey_z
NXP Employee
NXP Employee

hi,

1. According to the printed information, BL2 fails to start. There is an initialization conflict between fip.bin of BSP41 and the Bootloader you made, resulting in a start failure. Did you completely follow the configuration of AN13750? If you made some modifications, could you please give me more specific information? Or could you please provide me with your modified Bootloader project?
2.The ATF Load address in BSP41 is the same as that in BSP42. It should be noted that the Size is a little different, but it does not affect the result of starting kernal. When you have other changes to the initialization requirements, you need to modify the Bootloader project and then regenerate blob.bin.

BR

Joey

0 项奖励
回复
7,792 次查看
Allen_Cheng
Contributor II

Hi Joey,

 

All Configuration of the AN13750 are almost the same but I only modified:

1. u-boot : enable HSE and firmware path

2. ATF not apply mmc patch

3. remove m7_1 and m7_2 in bootloader

 

Attach files are bootlader and eb project.

Thanks.

 

Allen

0 项奖励
回复
7,761 次查看
Joey_z
NXP Employee
NXP Employee

hi,Allen_Cheng

Sorry for the late reply.
You can try Disable Secure Boot, as shown in the image below.

Joey_z_0-1734833365615.png

In addition, if you are not using mmc patch, make sure you modify the s32_common.mk file.

Wish it can help you.

BR

Joey

0 项奖励
回复
7,679 次查看
Allen_Cheng
Contributor II

Hi Joey,

 

I try to disable secure boot in EB tresos and disable HSE in u-boot.

But it looks like the same result.

 

Thanks.

标记 (1)
0 项奖励
回复
7,582 次查看
Joey_z
NXP Employee
NXP Employee

HI,Allen_Cheng

After investigation, this is a known issue as described in ALB-11457, and it has been resolved in Linux BSP42. The root cause lies in the bootloader de-initializes (in SysDal) the peripheral clocks before starting the applications, but s32_io_setup() is called without any prior initialization of the SDHC clocks from ATF. The description is shown in the BSP42 release note:

Joey_z_0-1736506523488.png

The easiest solution to fix this issue is recommending use BSP>=42. If continue working with BSP41, you can refer to these public commits to modify ATF code.

Hope it can help you.

BR

Joey

0 项奖励
回复
7,541 次查看
Allen_Cheng
Contributor II

Hi Joey,

Thanks for your help.

I will base on BSP42 for development.

 

Allen

0 项奖励
回复
7,613 次查看
Joey_z
NXP Employee
NXP Employee

hi,Allen_Cheng

Thank you for your reply.

I have reported the problem,and I will reply to you as soon as I have the result.

BR

Joey

0 项奖励
回复
%3CLINGO-SUB%20id%3D%22lingo-sub-2007887%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ES32G%20RDB2%20%E5%A4%9A%E6%A0%B8%E5%90%AF%E5%8A%A8%E5%9C%A8%20bsp41%20%E4%B8%AD%E6%8C%82%E8%B5%B7%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2007887%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3E%E6%82%A8%E5%A5%BD%EF%BC%8CNXP%E5%9B%A2%E9%98%9F%EF%BC%9A%3C%2FP%3E%3CBR%20%2F%3E%3CP%3E%E6%88%91%E5%B0%9D%E8%AF%95%E6%8C%89%E7%85%A7%20AN13750%20%E5%AE%98%E6%96%B9%E6%96%87%E6%A1%A3%E8%AE%BE%E7%BD%AE%E5%85%B7%E6%9C%89%20A53%20%E5%92%8C%20M7%20%E7%9A%84%E5%A4%9A%E6%A0%B8%E7%8E%AF%E5%A2%83%E3%80%82%3C%2FP%3E%3CP%3E%E6%88%91%E5%9C%A8%20bsp41%20%E4%B8%AD%E5%8F%91%E7%8E%B0%E4%BA%86%E4%B8%80%E4%B8%AA%E5%90%AF%E5%8A%A8%E9%97%AE%E9%A2%98%EF%BC%8C%E5%B9%B6%E4%B8%94%E6%88%91%E4%B9%9F%E4%BD%BF%E7%94%A8%20bsp42%20%E6%9D%A5%E6%BE%84%E6%B8%85%E3%80%82%3C%2FP%3E%3CP%3E%E4%BD%86%E6%98%AFBSP42%E5%8F%AF%E4%BB%A5%E6%88%90%E5%8A%9F%E5%90%AF%E5%8A%A8%E5%88%B0Linux%E5%86%85%E6%A0%B8%E3%80%82%3C%2FP%3E%3CP%3EBSP41%20%E5%B0%86%E5%A7%8B%E7%BB%88%E5%9D%9A%E6%8C%81%3C%2FP%3E%3CP%3E%3CFONT%20color%3D%22%23FF0000%22%3E%E5%BC%95%E5%AF%BC%E5%8A%A0%E8%BD%BD%E7%A8%8B%E5%BA%8F%200x2%20%E4%BB%8E%20QSPI%20%E5%8A%A0%E8%BD%BD%E7%9A%84%E5%BA%94%E7%94%A8%E7%A8%8B%E5%BA%8F%201%20%E5%9B%BE%E5%83%8F%E7%89%87%E6%AE%B5%200%E3%80%82%3C%2FFONT%3E%3CBR%20%2F%3E%3CFONT%20color%3D%22%23FF0000%22%3E%E5%BC%95%E5%AF%BC%E5%8A%A0%E8%BD%BD%E7%A8%8B%E5%BA%8F%200x2%20%E5%BA%94%E7%94%A8%E7%A8%8B%E5%BA%8F%20M7_0%20%E5%B7%B2%E5%8A%A0%E8%BD%BD%E3%80%82%3C%2FFONT%3E%3C%2FP%3E%3CP%3E%E6%88%91%E5%B0%86%E8%BF%99%E4%B8%A4%E4%B8%AA%E7%89%88%E6%9C%AC%E7%9A%84%E6%97%A5%E5%BF%97%E6%B7%BB%E5%8A%A0%E5%88%B0%E9%99%84%E4%BB%B6%E4%B8%AD%E3%80%82%3C%2FP%3E%3CP%3E%E6%82%A8%E8%83%BD%E5%B8%AE%E5%BF%99%E6%BE%84%E6%B8%85%E4%B8%80%E4%B8%8B%E8%BF%99%E4%B8%AA%E9%97%AE%E9%A2%98%E5%90%97%EF%BC%9F%3C%2FP%3E%3CP%3E%E8%B0%A2%E8%B0%A2%E3%80%82%3C%2FP%3E%3CBR%20%2F%3E%3CP%3E%E8%A5%BF%E5%8D%97%EF%BC%9A%3C%2FP%3E%3CP%3E%E9%9B%86%E6%88%90%E5%8F%82%E8%80%83%E7%A4%BA%E4%BE%8BS32G2202306%3C%2FP%3E%3CP%3EEB%2027.1%3C%2FP%3E%3CP%3ERTD%204.4_4.0.0_P05_HF01%3C%2FP%3E%3CP%3EHSE_FW%20S32G2XX_0_1_0_16%3C%2FP%3E%3CBR%20%2F%3E%3CBR%20%2F%3E%3CBR%20%2F%3E%3CBR%20%2F%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2008806%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%E5%9B%9E%E5%A4%8D%EF%BC%9AS32G%20RDB2%20%E5%A4%9A%E6%A0%B8%E5%90%AF%E5%8A%A8%E5%9C%A8%20bsp41%20%E4%B8%AD%E6%8C%82%E8%B5%B7%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2008806%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%E5%97%A8%EF%BC%8C%E4%B9%94%E4%BC%8A%EF%BC%8C%3CBR%20%2F%3E%3CBR%20%2F%3E%20ATF%20%E5%8A%A0%E8%BD%BD%E5%9C%B0%E5%9D%80%E5%9C%A8%20bsp41%2Fbsp42%20%E4%B8%AD%E6%98%AF%E7%9B%B8%E5%90%8C%E7%9A%84%E3%80%82%3CBR%20%2F%3E%E5%85%A5%E5%8F%A3%E7%82%B9%E6%98%AF0x34700000%E3%80%82%3CBR%20%2F%3E%E8%B0%A2%E8%B0%A2%E3%80%82%3CBR%20%2F%3E%3CBR%20%2F%3E%E8%89%BE%E4%BC%A6%3CBR%20%2F%3E%3C%2FLINGO-BODY%3E