S32DS build S32G3 Port Demo IVT RAM start pointer error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS build S32G3 Port Demo IVT RAM start pointer error

270 Views
Wzlinux
Contributor III

HI dear NXP

i am using S32G3 RDB3 building the demp example.  and build pass get the bin.

and i get the init_sram address from the linker file.

but when i fill this value to RAM start pointer. S32DS resopnse the value is error. 

please help to take a look at .

thanks.

Wzlinux_0-1741863204749.png

 

0 Kudos
Reply
1 Reply

213 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Wzlinux 

Sorry for the late response.

I checked it with the same examples from my side, and do not meet such issues(RTD4.0.2HF3), may I know which version RTD/S32DS used in your test? any modifications made on the default settings/codes?

What is the prints from "problems" at the bottom of the picture? I cannot see the details.

 

BR

Chenyin

0 Kudos
Reply