S32 Flash Tool failed in S32G-VNP-RDB3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32 Flash Tool failed in S32G-VNP-RDB3

跳至解决方案
2,086 次查看
neilpatrick32
Contributor I

Hi NXP Community,

I am using the S32G-VNP-RDB3 evaluation board (S32G399A).

According to "UGS32G-VNP-RDB3" I configured the DIP Switches following the "3.2 Default Switch Setting" setting, but also change for the "3.7 Switch Setting for Serial Boot"

3.2 Default Switch Setting.JPG

3.7 Switch Setting for Serial Boot.JPG

Settings for the UART COM which is connected to UART0.

UART settings.JPG

Then i followed the procedure from "AN13727", but i got this error always.

S32 Flash tool.JPG

The light from the UART0 is visible whenever uploading to the target.

Could you please support me? Thanks!

1 解答
2,060 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We have seen that there is a ticket under the ticket support, which we have answered to it.

Still, we seem to have missed some information. We have our COM set with the following properties:

DanielAguirre_0-1691174353307.png

If you set your COM with 9600 baudrate does it happen the same? If you like to continue your support on the NXP support case we do not have any problem.

Please, let us know.

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,061 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We have seen that there is a ticket under the ticket support, which we have answered to it.

Still, we seem to have missed some information. We have our COM set with the following properties:

DanielAguirre_0-1691174353307.png

If you set your COM with 9600 baudrate does it happen the same? If you like to continue your support on the NXP support case we do not have any problem.

Please, let us know.

0 项奖励
回复